Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum GPIO Safety Tips?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 690 subscribers
  • Views 1791 views
  • Users 0 members are here
  • raspberry_pi
Related

GPIO Safety Tips?

Former Member
Former Member over 12 years ago

I got a Pi over Christmas, installed Raspbian on it and am able to talk to it via wireless over SSH. So far so good. Now to do something with it.

When I picked it up, I got the breadboard connector to go with it. I could spend an addition $35 and get a PiFace Digital, but I was hoping to use it raw for at least a while, and use the general GPIO pins directly, rather than doing everything through the SPI.

 

Aside from avoiding excessive voltages, excessive supply current draw, and static discharge, are there any particular things to look out for when working with the GPIO pins?

Are there any common situations when working with circuits that I should be particularly sensitive to so I don't brick the thing?

 

For instance, one thing that occurs to me is that, if feasible, I should power my circuit from the Pi to ensure my circuit isn't on when the Pi isn't on and that it never operates off of a voltage even marginally higher than the Pi. Which raises the additional question: Is the Pi tremendously sensitive to power sequencing? I don't want to let the magic smoke out. image

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    Before you hook anything up, read the RasPi Hardware Wiki.  It includes a lot of good specs and safety tips, along with programming examples.

     

    IMO go ahead and use the 3.3V supplied by RasPi over the GPIO connector.  You can draw 50 mA, which is enough for a lot of LEDs at 2 mA each, and input switches use less than 1 mA for the pull-up.  If you're going to power something big, you've got to use transistors and/or relays and have a separate voltage supply, with common ground.  Darlington pairs are a great way to switch a lot of current.  Be sure to include flyback diodes for inductive loads like motors, relays, and speakers.

     

    Be very careful with the GPIO's 5V pins.  If you short them to something else, you can permanently kill your RasPi.  I recommend covering them with bits of wire insulation to prevent a slipped probe from causing tragedy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to johnbeetem

    Many thanks, John, for the pointer to the Wiki and the links that split off from there, especially about level converters. I guess 7407s are my friends as well as being inexpensive and easy to swap out as a sacrificial victim when I'm experimenting. (It isn't just about not letting the magic smoke out - it's who's magic smoke you're letting out. image) I'll also have to read the processor manual (or portions thereof) for some of the hardware detail, although the drivers will shield me from some of the *really* interesting stuff.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago in reply to johnbeetem

    Many thanks, John, for the pointer to the Wiki and the links that split off from there, especially about level converters. I guess 7407s are my friends as well as being inexpensive and easy to swap out as a sacrificial victim when I'm experimenting. (It isn't just about not letting the magic smoke out - it's who's magic smoke you're letting out. image) I'll also have to read the processor manual (or portions thereof) for some of the hardware detail, although the drivers will shield me from some of the *really* interesting stuff.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to Former Member

    Ralph Mack wrote:

     

    Many thanks, John, for the pointer to the Wiki and the links that split off from there, especially about level converters. I guess 7407s are my friends as well as being inexpensive and easy to swap out as a sacrificial victim when I'm experimenting. (It isn't just about not letting the magic smoke out - it's who's magic smoke you're letting out. ) I'll also have to read the processor manual (or portions thereof) for some of the hardware detail, although the drivers will shield me from some of the *really* interesting stuff.


    I'm not sure 7407s are your friends.  If they're 5V TTL parts, they pull their inputs high.  I don't know if the voltage and current from a TTL input would be high enough to damage RasPi, but I'd play it safe and stick to driving transistors.  External CMOS drivers such as 74HCT or 74ACT should be OK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer