Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi sd card issues
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 680 subscribers
  • Views 2302 views
  • Users 0 members are here
  • raspberry-pi
  • sdcard
Related

Raspberry pi sd card issues

Former Member
Former Member over 11 years ago

Even when everything is connected, my rasberry pi won't boot up. The pc (macbook pro) I am using as a display just stays on its normal screen. I suspect that this problem has something to do with my NOOBS-installed, formatted sd card, which will not load onto the pc even inserted properly into the sd slot, so I had to use a card reader to set it up. For some reason the sd card works only with the reader. Do you guys have any advice on what is causing this problem, and if so, what I can do about it?

  • Sign in to reply
  • Cancel
Parents
  • mazzmn
    0 mazzmn over 11 years ago

    Hi Liam

    this sounds like something I ran into with an XBMC SD card. I would try a couple of things:

    First take a look at the symptoms of the boot failure (ie any lights flashing, screen displayed, etc??) and compare that to this debug page
    R-Pi Troubleshooting - eLinux.org 

    Or, create another, new NOOBs SD card and try to use that one....this is what worked for me

    Good Luck, let us know how it goes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to mazzmn

    What I thought was an sd card is actually a micro-sd adapter, but it is specifically made for the pi, and I ordered it from element 14 / newark so it should be compatible with the pi. It is also brand new. When I plug it into the pi the green led on the pi glows softly, but not very brightly. Thanks for all of the help so far!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • annatoli529
    0 annatoli529 over 11 years ago in reply to Former Member

    HI Liam your response seems to remind me with an issue I had with my first PSP. It doesn't use isr SD cards but I used an adapter that made a conversion to SD. I bought two of them I has two PSPs and ond worked fine the second didn't so prrhaps you could change the adapter too and make ot work. My point is your weak glow of the green LED seems like a contact issue that my problem too. But I guess uou tried this option by now. Anyway goodluck and keep us up to date with your progress.

    Annatoli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to Former Member

    Liam Brent-Hurst wrote:

     

    What I thought was an sd card is actually a micro-sd adapter, but it is specifically made for the pi, and I ordered it from element 14 / newark so it should be compatible with the pi. It is also brand new. When I plug it into the pi the green led on the pi glows softly, but not very brightly. Thanks for all of the help so far!

    The green LED glowing faintly means that RasPi hasn't executed any boot code yet: see the RasPi Troubleshooting Wiki.  The green LED will probably do the same thing without the Micro SD adapter plugged in.

     

    This is a silly question, but you do have a Micro SD card in the adapter, right?  If so, maybe the Micro SD card is bad or the image wasn't copied properly.  Check the Troubleshooting Wiki for most of the things that go wrong with RasPi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to johnbeetem

    John Beetem, it does do the same thing without the adapter. And yes, I do have the Micro SD in the adapter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to Former Member

    Liam Brent-Hurst wrote:

     

    John Beetem, it does do the same thing without the adapter. And yes, I do have the Micro SD in the adapter.

    Any luck with the RasPi Troubleshooting Wiki at  R-Pi Troubleshooting - eLinux.org?

    There are quite a number things that can go wrong.  The most common is power supply problems, often due to a Micro USB cable with conductors that are too thin.  It's also possible that your SD card image wasn't written correctly.  If only the red LED is on and the green is only dim, it means that for whatever reason the RasPi boot ROM in the SoC isn't able to find a valid executable image on the SD card.

     

    Do try booting with no peripherals attached.  If the green LED flashes a bunch of times in the first 20 seconds or so, it means that the SD card is being read.  If this is the case, a peripheral is loading down the power supply: plug them in one by one to see which one prevents RasPi from operating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to Former Member

    Liam Brent-Hurst wrote:

     

    John Beetem, it does do the same thing without the adapter. And yes, I do have the Micro SD in the adapter.

    Any luck with the RasPi Troubleshooting Wiki at  R-Pi Troubleshooting - eLinux.org?

    There are quite a number things that can go wrong.  The most common is power supply problems, often due to a Micro USB cable with conductors that are too thin.  It's also possible that your SD card image wasn't written correctly.  If only the red LED is on and the green is only dim, it means that for whatever reason the RasPi boot ROM in the SoC isn't able to find a valid executable image on the SD card.

     

    Do try booting with no peripherals attached.  If the green LED flashes a bunch of times in the first 20 seconds or so, it means that the SD card is being read.  If this is the case, a peripheral is loading down the power supply: plug them in one by one to see which one prevents RasPi from operating.