Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Heat Treatment Oven
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 2 answers
  • Subscribers 709 subscribers
  • Views 2589 views
  • Users 0 members are here
  • raspberry_pi
Related

Heat Treatment Oven

e14 Contributor
e14 Contributor over 12 years ago

Hi All

I wish to build a heat treatment oven/forge. The main use for it would be heat treatment of wood working tools but i would also like to be able to use it to make Mokume-gane so i need it to be fully electrical so i can flood the heating chamber with inert gases such as argon or co2/argon mix. I would like to be able to make the elements and gases flow rate fully programmable. Which would be better for use raspberry pi or aurdino

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    Sure, you want your DS channel current to be significantly greater than your actual current.  This is part of the DC analysis.  MOSFETs at these bias levels have positive tempcos and we don't want to warm them up into a regime where they perform poorly and burn fingers.

     

    The issue with quenching spikes is not about DC current levels in the conduction channel whatsoever, it is about the competing parameter, channel breakdown voltage (and AC analysis) when the channel isn't enhanced.  The inductive load will spend its magnetic field attempting to maintain the current through it (and anything in series with it)  when anything acts to change that current.  The spike tapers off logarithmically because its energy source is in the past.  But at the moment of disruption, the current is maintained.  If our Q suddenly goes High-Z, the drain potential will spike to maintain the current level through the conduction channel.  Quenching is about finding an alternate route for this current, so that our voltage spike at turnoff doesn't rise to Q BV.

     

    Varicaps are devices used to tune stuff in RF, like VCOs for PLLs and resonant traps.

     

    Given like technology, diode capacitance is a convenient way to express speed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago

    Sure, you want your DS channel current to be significantly greater than your actual current.  This is part of the DC analysis.  MOSFETs at these bias levels have positive tempcos and we don't want to warm them up into a regime where they perform poorly and burn fingers.

     

    The issue with quenching spikes is not about DC current levels in the conduction channel whatsoever, it is about the competing parameter, channel breakdown voltage (and AC analysis) when the channel isn't enhanced.  The inductive load will spend its magnetic field attempting to maintain the current through it (and anything in series with it)  when anything acts to change that current.  The spike tapers off logarithmically because its energy source is in the past.  But at the moment of disruption, the current is maintained.  If our Q suddenly goes High-Z, the drain potential will spike to maintain the current level through the conduction channel.  Quenching is about finding an alternate route for this current, so that our voltage spike at turnoff doesn't rise to Q BV.

     

    Varicaps are devices used to tune stuff in RF, like VCOs for PLLs and resonant traps.

     

    Given like technology, diode capacitance is a convenient way to express speed.