Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum need .py code for reading Max31855 A/D temp converter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 32 replies
  • Answers 2 answers
  • Subscribers 709 subscribers
  • Views 6322 views
  • Users 0 members are here
  • raspberry_pi
  • raspberrypi
  • adafruit
Related

need .py code for reading Max31855 A/D temp converter

donb
donb over 12 years ago

Thru this site I got info on a Adafruit Max31855 module. Now does anyone have the code necessary to read the digital output of this fine little module? I don't have the experience to write the code, but truly need the code to save a very long and steep learning curve.   Don

  • Sign in to reply
  • Cancel
Parents
  • iagorubio
    0 iagorubio over 12 years ago

    You can even compile that code to work with the raspberry with the arduPi library Cooking Hacks - Documentation - Raspberry Pi to Arduino shields connection bridge or may be with the WiringPi library.

     

    You just will need to add a main() function as entry point for you progra, initialize one Adafruit_MAX31855 instance and call the readCelsius() or readFarenheit() methods.

     

    There is one thing I would double check before to connect it, from the description you can read "This breakout board has the chip itself, a 3.3V regulator with 10uF bypass capacitors and level shifting circuitry". Take care, the Raspberrry is a 3.3V device itself, you don't need level shifting at all.

     

    Before to start I would input 3.3V in both VIN and V3.3 and check if the output is 3.3V or you risk a fried Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • donb
    0 donb over 12 years ago in reply to iagorubio

    Thanks Michael, I will take a stab at it. I am assuming that the .ccp code is similar to the .py code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • donb
    0 donb over 12 years ago in reply to iagorubio

    Thanks Michael, I will take a stab at it. I am assuming that the .ccp code is similar to the .py code.