Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum External 5v supply  instructions missing in user manual?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 706 subscribers
  • Views 941 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

External 5v supply  instructions missing in user manual?

superpat
superpat over 12 years ago

Hi,

 

I am making the assumption that one can power the audio card AND the Pi from the Aux 5V jack, thus avoiding the need for TWO power supplies.

 

Just tried to use the Wolfson audio card with external 5V supply (5v Aux), so I can try the integrated speaker amplifiers.

 

It will not work  without adding a link or 0 ohm resistor  R44, located by the side of the 5v jack socket. without this link, the aux 5v does NOT feed the internal 3.3 and 1.8 v regs.

 

(see schematic diagrams.....  R44 is marked as DNP  do not populate, )

 

The  user  manual states that one has to add terminations for the speaker cables and also

 

 It is necessary to supply auxiliary power to the Audio Card in order to drive
external loudspeakers. An external power supply with output voltage of 5V,
current delivery capability of 2,000mA, a centre positive power plug of internal
diameter 2.1mm, and external diameter 5.5mm.

 

But there is nothing about  inserting 0 ohm or link in R44

 

SHOULD THERE BE?

 

Also, adding a link to R44 position is not for the inexperienced solderer! It's a 0603  size component.

 

regards

 

Patrick

 

Message was edited by: Patrick Keane

  • Sign in to reply
  • Cancel
Parents
  • superpat
    0 superpat over 12 years ago

    Hi,

     

    Re-reading my last post I realised I had not fully stated the result  of connecting R44 and the  5v Aux


    So,,,,, I made a solder bridge on the Audio card at R44 position,  couldn't find a 0 ohm  SMD in my parts box.

     

    Stuck a 5v jack in the Audio card socket, with NO other PI connected power supply.

     

    It all works well, Pi  boots and  ausio works great,  i.e. running MPD and playing flacs onto line out.

     

    I have not tried  the loudspeaker outputs yet, I have to find a pair of small speakers in my junk box. I have a pair of Warfdale bookshelf speakers to hand  but they are marked 75W, I don't think a 1.4 W o/p will drive them very well!

     

    cheers

     

    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • richardbeattie
    0 richardbeattie over 8 years ago in reply to superpat

    Hi,

     

    I am also looking at getting the aux power to power the Raspberry Pi. I am just wondering would you have a schematic diagram of where exactly you put the solder bridge, I am inexperienced at this and so was able to see from your post where the bridge/resistor is meant to go

     

    Thanks,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago in reply to richardbeattie

    I am going with a USB speaker and avoid the mess. Not digital, but who needs that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago in reply to richardbeattie

    I am going with a USB speaker and avoid the mess. Not digital, but who needs that.