Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum How good does the Wolfson Audio Card fit onto the Raspberry PI ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 704 subscribers
  • Views 901 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

How good does the Wolfson Audio Card fit onto the Raspberry PI ?

e14 Contributor
e14 Contributor over 12 years ago

I recently received a Raspberry PI and a Wolfson Audio Card to suit. When I fitted the audio card to the PI I noticed a couple of problems.

1. The P5 connection looks to be incomplete, the pins only protrude halfway into the circuit board holes.

2. The underside of the EX Connector on the audio card sits hard on the PI headphone socket bending the audio card board up.

I have not powered the boards up yet, or installed any operating system, so can't comment on operation yet.

Anyone have simular experience or comments.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    1. I think that's how it's supposed to be. The pins are not meant to go into the holes, but make contact with the "rim".

    2. Mine is the same. The board sits on the headphone connector and bends slightly when I tighten the nylon screw.

     

    I haven't applied power to mine either, yet. Still about 8 hours to go on the kernel build...

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mertresvag
    0 mertresvag over 12 years ago in reply to e14 Contributor

    This is after my meaning a bad design. I assembled the Wolfson card and the PI after the instruction in the manual, I cleaned the contacts with 96% alcohol. But I never got to work. So now I'm returning it to my supplier. I'll wait for a better design for this P5 connection.

     

    Regards Magne.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mertresvag
    0 mertresvag over 12 years ago in reply to e14 Contributor

    This is after my meaning a bad design. I assembled the Wolfson card and the PI after the instruction in the manual, I cleaned the contacts with 96% alcohol. But I never got to work. So now I'm returning it to my supplier. I'll wait for a better design for this P5 connection.

     

    Regards Magne.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mertresvag

    Since I posted the original question I have loaded a SD card with the image supplied by Wolfson, powered up  the PI. Everything appears to working Ok, able to play audio files via line out, record audio files via line in. No problems so far, however my question still stands. No comment from Wolfson via this forum yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I assembled the board per instructions and loaded the drivers and then Pianobar. I think the fit is very good and the board works very well. I compiled the image from scratch and everything worked great.

     

    BRyan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mikepowell
    0 mikepowell over 12 years ago in reply to e14 Contributor

    The board is designed this way. The 'pogo' pins on the Wolfson Audio Card extend down to the P5 pads, and they are cupped by the edges of the gold plated holes at that connector position. They are not designed to travel through the holes, else there would be a risk that no connection would be made if that happened.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mikepowell

    Thanks Mike for the explanation of the P5 connection.

    With reference to the circuit board sitting hard on the external connection header pins, I trimmed / cut the pins on the underside of the header, which alleviated some of the pressure on the board, hence there is only a slight bend in the board now.