Raspberry Pi Forum Wolfson modified Noobs raspbian zipped img  Cannot unzip new download
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 108 replies
  • Subscribers 692 subscribers
  • Views 17987 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Wolfson modified Noobs raspbian zipped img  Cannot unzip new download

superpat
superpat over 11 years ago

Hi,

 

I deleted my original zip download  and the img of the above file.   I have downloaded it again, but all the unzip programs I try will not unzip it, ( say no unzip sig).

 

I have painfully downloaded it again and still no joy with unzipping.

 

Have you changed the file recently?

 

Please, please  publish the md5 sum for this file!  (so I can eliminate download errors)

 

many thanks

 

regards

 

Patrick

  • Sign in to reply
  • Cancel
Parents
  • superpat
    0 superpat over 11 years ago

    Please make the md5 checksum for this file available.

     

    Thank you

     

    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to superpat

    I have kept my original download, but I have downloaded the zip file again to compare them.

    I'm running WinXP with Cygwin.

    My old download from Feb 26 and today's are identical.

    $ ls -ltr *wolfson*zip
    -rwx------+ 1 ragnar Ingen 4713117059 Feb 26 12:16 wolfson_3.10_master.zip
    -rwx------+ 1 ragnar Ingen 4713117059 Mar 17 21:12 new_wolfson_3.10_master.zip
    $ md5sum wolfson_3.10_master.zip new_wolfson_3.10_master.zip
    72d091a9b43e47a5b7b85432ec15611c *wolfson_3.10_master.zip
    72d091a9b43e47a5b7b85432ec15611c *new_wolfson_3.10_master.zip

     

    WinZip complains - "Archive is greater than 4 gigabytes."

    WinRAR complains - "! ... wolfson_3.10_master.zip: Either multipart or corrupt ZIP archive"

    Command line unzip complains - "warning [wolfson_3.10_master.zip]: 418149653 extra bytes at beginning or within zipfile...error [wolfson_3.10_master.zip]: start of central directory not found;...

    7-zip works, it extracts the image OK.

     

    There are Linux and OSX versions of 7-zip available at http://www.7-zip.org/download.html

    --

    Ragnar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    You have my kernel installed OK and the Wolfson card is visible as card 0.

    snd_rpi_wsp is the Wolfson and bcm2835 is the Raspberry's built-in audio.

    So far, so good.

     

    But the message "the audio device "default" could not be used: Device or resource busy" indicates that some other audio player is occupying the Wolfson card.

    Which audio applications have you installed? Some install a server daemon that starts automatically at boot and claims the sound card for itself.

    To find out which app that is using the sound card run this command:

    fuser -v /dev/snd/*

     

    And I'm still interested in your ~/.asoundrc image

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Ive installed two other programs other than the ones you suggested in the desktop text file, VLC and Audacity.

     

    And I found the tilde:

     

    pi@raspberrypi ~ $ cat ~/.asoundrc
    #######################################################################
    #
    # Wolfson Audio Card for Raspberry Pi
    #
    pcm.wolfson_pi_soundcard {
       type hw
       card sndrpiwsp
       device 0
    }

    pcm.softvol {
       type            softvol
       slave {
           pcm         "wolfson_pi_soundcard"
       }
       control {
           name        "Master"
           card        0
       }
    }

    pcm.!default softvol


    oddly I don't see snd in VLC anymore. And I still can't get anything from the 3.5 jack. Any advice? Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Your ~/.asoundrc looks OK.

    And I still can't get anything from the 3.5 jack.

    Which jack is that? A RPi with Wolfson has four 3.5 jacks.

    You did remember to run the "Playback_to...sh" script to put sound on the output you want?

     

    Try playing something from the command line with aplay:

    aplay -vv some_file.wav
    aplay -vv -Dhw:1 some_file.wav # This will try to play on the RPi's built-in audio

    and post the output.

     

    And the output from

    fuser -v /dev/snd/* 

    when no audio applications are running.

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    ./Playback_to_Headset.sh

    bash: ./Playback_to_Headset.sh: No such file or directory

     

    and when I typed "fuser -v /dev/snd/*" into terminal I get nothing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    The use case scripts reside in the folder use_case_scripts.

    Either

    cd ~/use_case_scripts
    ./Playback_to_Headset.sh

    or

    ~/use_case_scripts/Playback_to_Headset.sh

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member
    1. cd ~/use_case_scripts 
    2. ./Playback_to_Headset.sh  

     

    all I got was this as a result:

     

    amixer: Cannot find the given element from control hw:0 (but the same thing for 11 lines)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    It looks like the RPi has lost the connection to the Wolfson card.

    Does any of the other scripts run without error messages?

    Post the  output of these commands:

    aplay -l

    aplay -L

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    яков х wrote:

     

    1. cd ~/use_case_scripts
    2. ./Playback_to_Headset.sh 

     

    all I got was this as a result:

     

    amixer: Cannot find the given element from control hw:0 (but the same thing for 11 lines)

     

    There was a thread about the same error message (on running './Playback_to_Headset.sh')  back in March

     

    Problem getting Wolfson Audio Card working: "amixer: Cannot find the given element from control hw:0"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Yep, and that turned out to be a broken Wolfson card.image

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Oh how odd. It was working fine before with the official wolfson image. I just couldn't expand the filesystem to the entire 16gb card. I will have to retry the official image when I have time later... ugh I hate wearing down flash storage.

     

    Although I must add something regarding the contact of the p5 connections on the wolfson card. This seems challenging considering there is soldering on the audio card above the blue RPI 3.5 mm audio jack that protrudes, preventing the audio card to fit easily. Could this be the culprit?

     

    On the other hand I saw that someone performed an rpi-update, like myself. This could be the issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Oh how odd. It was working fine before with the official wolfson image. I just couldn't expand the filesystem to the entire 16gb card. I will have to retry the official image when I have time later... ugh I hate wearing down flash storage.

     

    Although I must add something regarding the contact of the p5 connections on the wolfson card. This seems challenging considering there is soldering on the audio card above the blue RPI 3.5 mm audio jack that protrudes, preventing the audio card to fit easily. Could this be the culprit?

     

    On the other hand I saw that someone performed an rpi-update, like myself. This could be the issue.