Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wolfson modified Noobs raspbian zipped img  Cannot unzip new download
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 108 replies
  • Subscribers 714 subscribers
  • Views 20156 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Wolfson modified Noobs raspbian zipped img  Cannot unzip new download

superpat
superpat over 12 years ago

Hi,

 

I deleted my original zip download  and the img of the above file.   I have downloaded it again, but all the unzip programs I try will not unzip it, ( say no unzip sig).

 

I have painfully downloaded it again and still no joy with unzipping.

 

Have you changed the file recently?

 

Please, please  publish the md5 sum for this file!  (so I can eliminate download errors)

 

many thanks

 

regards

 

Patrick

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I am experiencing the same problem. I have downloaded http://downloads.element14.com/wolfson/wolfson_3.10_master.zip onto two different computer systems, and on both systems get the following error message when using unzip to unpack the file:

     

    sh-4.2$ unzip wolfson_3.10_master.zip

    Archive:  wolfson_3.10_master.zip

    warning [wolfson_3.10_master.zip]:  418149653 extra bytes at beginning or within zipfile

      (attempting to process anyway)

    error [wolfson_3.10_master.zip]:  start of central directory not found;

      zipfile corrupt.

      (please check that you have transferred or created the zipfile in the

      appropriate BINARY mode and that you have compiled UnZip properly)

     

    Has anyone unzipped this file succesfully? Which version of unzip or other archive program did you use?

     

    Thanks,

     

    Geordie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    I've not tried it on the file you mention, but on other zip files occasionally Windows in-built unzipping capability fails.

    WinZip comes with nags and bloatware, and is really not recommended either.

    7-zip has never failed for me. It may be worth a try.

    On Linux I just use built-in unzip CLI utility.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    In both cases I used unzip on the command line. I also unzipped it with "The Unarchiver" on MacOS 10.7.4. That didn't work either. Unfortunately I don't have a Windows installation so I can't try 7-zip...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • superpat
    0 superpat over 12 years ago

    Please make the md5 checksum for this file available.

     

    Thank you

     

    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to superpat

    I have kept my original download, but I have downloaded the zip file again to compare them.

    I'm running WinXP with Cygwin.

    My old download from Feb 26 and today's are identical.

    $ ls -ltr *wolfson*zip
    -rwx------+ 1 ragnar Ingen 4713117059 Feb 26 12:16 wolfson_3.10_master.zip
    -rwx------+ 1 ragnar Ingen 4713117059 Mar 17 21:12 new_wolfson_3.10_master.zip
    $ md5sum wolfson_3.10_master.zip new_wolfson_3.10_master.zip
    72d091a9b43e47a5b7b85432ec15611c *wolfson_3.10_master.zip
    72d091a9b43e47a5b7b85432ec15611c *new_wolfson_3.10_master.zip

     

    WinZip complains - "Archive is greater than 4 gigabytes."

    WinRAR complains - "! ... wolfson_3.10_master.zip: Either multipart or corrupt ZIP archive"

    Command line unzip complains - "warning [wolfson_3.10_master.zip]: 418149653 extra bytes at beginning or within zipfile...error [wolfson_3.10_master.zip]: start of central directory not found;...

    7-zip works, it extracts the image OK.

     

    There are Linux and OSX versions of 7-zip available at http://www.7-zip.org/download.html

    --

    Ragnar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • superpat
    0 superpat over 12 years ago in reply to e14 Contributor

    Hi Ragnar,

     

    The first time I downloaded the file and uzipped it, I used my LInux box, and I had no problems,  I think, (not sure)  I have rebuilt the Linux system in the meantime, (which I do quite often),  and moved from pure Debian to a  Mint  distro.

     

    Unfortunately, I cannot remember whether the Deb system had any 'special' unzippers installed, or how I unzipped it the first time.

     

    I know that with the current system,  I cannot use the standard cli unzip,  or the gui un-archiver, (I don't know whether that is a wrapper for the standard unzip).

     

    I will try your recommendation later.

     

    thanks

     

    regards

     

    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to superpat

    At least in the Ubuntu and Raspbian repositories, there are 7-zip packages available.

    p7zip - 7z file archiver with high compression ratio

    p7zip-full - 7z and 7za file archivers with high compression ratio

     

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I successfully unzipped the file on MacOS using Keka ( Keka - the free Mac OS X file archiver ).
    Ben.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Sadly, 7-zip on macos 10.7.4 fails to open the file as well. "Keka" fails with the following error:

     

    Extraction of wolfson_3.10_master.zip failed

    Error code 2 using "p7zip"

    Fatal error

     

    In the absence of any customer support whatsoever from Element14/Newark and Wolfson Microelectronics I guess I'll just try downloading the next macos version of 7-zip from http://www.7-zip.org/download.html

     

    This product - the audio card -  sure is Mickey Mouse! Can it be that the it requires windows in order to work? It would have been helpful if they had said that up front.

     

    I just want to use the card that I paid them good money for.

     

    Thanks, Ragnar and Benjamin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaddoux
    0 dmaddoux over 12 years ago

    I'm having the same problem. The download process shows that the image file is supposed to be 4.4gb yet only 480mb is all that's downloaded. Is this correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>