Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Problem getting Wolfson Audio Card working: "amixer: Cannot find the given element from control hw:0"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 707 subscribers
  • Views 4201 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Problem getting Wolfson Audio Card working: "amixer: Cannot find the given element from control hw:0"

e14 Contributor
e14 Contributor over 12 years ago

I'm having problems getting my new wolfson audio card working. I've following the instructions in the manual when installing the card, and I'm using the custom supplied Noobs image.

 

When using the Playback_to_Headset.sh script I get the error message:

 

amixer: Cannot find the given element from control hw:0

 

Suspecting the card was not correctly seated, I took it apart and rebuilt it. When inspecting the P5 connector, there seems to be good contact between the spring-loaded pillars and the raspberry pi board. I've also successfully checked continuity between the solder joints on the wolfson card and the pads on the back of the pi board. The nylon screw is securely fastened.

 

Has anyone else had this problem? Is there anything I can do to investigate further.

 

The only other clues are these lines in syslog:

 

Feb 12 20:24:17 raspberrypi kernel: [    5.172128] snd-rpi-wsp snd-rpi-wsp.0: ASoC: can't create pcm WM5102 AiFi :-517

Feb 12 20:24:17 raspberrypi kernel: [    5.183446] snd-rpi-wsp snd-rpi-wsp.0: ASoC: failed to instantiate card -517

Feb 12 20:24:17 raspberrypi kernel: [    5.204848] snd-rpi-wsp snd-rpi-wsp.0: Failed to register card: -517

 

The D3 green LED is lit on the board when powered, and the D1 red LED is unlit. The only other device I have connected is a USB keyboard.

 

Cheers in advance.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I too am having the same problem, after upgrading and configuring my project.

     

    Flashing the modified noob image downloaded from here gets rid of the red light, regrettably my project doesn't allow me to test the sound as I don't have a HDMI screen in the same room as the SPDIF amp..

     

    I hope a solution can be found so that I can re-flash my project saving me hours of development time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I too am having the same problem, after upgrading and configuring my project.

     

    Flashing the modified noob image downloaded from here gets rid of the red light, regrettably my project doesn't allow me to test the sound as I don't have a HDMI screen in the same room as the SPDIF amp..

     

    I hope a solution can be found so that I can re-flash my project saving me hours of development time.