Raspberry Pi Forum Wolfson Audio Capture With DarkIce, How?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Subscribers 676 subscribers
  • Views 3852 views
  • Users 0 members are here
  • wolfson
  • alsa
  • darkice
  • raspberry_pi
  • raspeberry_pi_accessories
  • icecast
Related

Wolfson Audio Capture With DarkIce, How?

Former Member
Former Member over 11 years ago

Hi all, so I received my Wolfson a few weeks ago and finally got round to working with it image

 

I'm trying to put together an Icecast Source Client via the pi, previously without the wolfson it would glitch and generally cause a substandard broadcast, so I'm hoping with the wolfson I can make a nice cost effective broadcast box.

 

However, I downloaded the wheezy image (Re: Wolfson modified Noobs raspbian zipped img  Cannot unzip new download) with the precompiled drivers in and duely set off compiling Darkice with MP3 support (Live mp3 streaming from audio-in with DarkIce and Icecast2 on Raspberry Pi)

 

My problem however is I've tried selecting the correct device but I just dont know which one it is.

 

I've executed the Record_from_lineIn.sh script to start with and then tried arecorder -l which returns:

**** List of CAPTURE Hardware Devices ****

card 0: sndrpiwsp [snd_rpi_wsp], device 0: WM5102 AiFi wm5102-aif1-0 []

  Subdevices: 1/1

  Subdevice #0: subdevice #0

so I've tried entering hw:0,0 into the darkice.cfg device line and I get the following:

Using config file: /etc/darkice.cfg

Using ALSA DSP input device: hw:0,0

Could not set POSIX real-time scheduling, this may cause recording skips.

Try to run darkice as the super-user.

DarkIce: AlsaDspSource.cpp:173: can't set channels [1]

(also tried it sudo'd but no change)

 

I've also tried device = default but get the same error, also tried options such as snd_rpi_wsp, sndrpiwsp but cant get it to capture effectively.

 

Any ideas what the capture device should be set as for the line in at all (as a start image)

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Hi Leigh!

    Look for channel = 1 in the configuration file. The Wolfson card won't allow anything other than 2 channels.

    This is my darkice.cfg, which works splendidly, streaming mp3: (server name and password have been changed to protect the guilty...)

    [general]
    duration = 0 # duration of encoding, in seconds. 0 means forever
    bufferSecs = 5 # size of internal slip buffer, in seconds
    reconnect = yes # reconnect to the server(s) if disconnected
    
    # this section describes the audio input that will be streamed
    [input]
    device = hw:0,0 # ALSA device
    sampleRate = 44100 # sample rate in Hz. try 11025, 22050 or 44100
    bitsPerSample = 16 # bits per sample. try 16
    channel = 2 # channels. 1 = mono, 2 = stereo
    
    # this section describes a streaming connection to an IceCast2 server
    [icecast2-0]
    format = mp3 # format of the stream: MP3
    bitrateMode = cbr # constant bit rate
    bitrate = 256 # bitrate of the stream sent to the server
    quality = 0.8
    server = www.example.local # host name of the server
    port = 8000 # port of the IceCast2 server, usually 8000
    password = xxxxxx # source password to the IceCast2 server
    mountPoint = liveob # mount point of this stream on the IceCast2 server
    sampleRate = 44100
    channel = 2 # Stereo
    name = OB case # name of the stream
    description = Live from the field # description of the stream
    url = http://www.example.com/liveob # URL related to the stream
    genre = Speech # genre of the stream
    public = no # advertise this stream?
    #localDumpFile = dump.ogg # local dump file

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks for that - spot on! that was easy and I've been streaming now for the last hour without a glitch so looks as it its done the trick!

     

    Darkice seems to be consuming approx 50% cpu at the moment as a point of reference - thats streaming a 96k/44100/stereo/abr track the whole time.

     

    Thanks very much image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks for that - spot on! that was easy and I've been streaming now for the last hour without a glitch so looks as it its done the trick!

     

    Darkice seems to be consuming approx 50% cpu at the moment as a point of reference - thats streaming a 96k/44100/stereo/abr track the whole time.

     

    Thanks very much image