Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is it possible to send audio from "SPDIF In" to the Lineout using the mixer?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 3 answers
  • Subscribers 709 subscribers
  • Views 4500 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Is it possible to send audio from "SPDIF In" to the Lineout using the mixer?

eveready1010
eveready1010 over 12 years ago

I have been trying to figure this out for a while now...

 

I can record audio coming in from the "SPDIF In" to a file, and then I can play back the same file to the Lineout, but is it possible to "mix" the incoming audio from the SPDIF In to the Lineout only using the mixer?

 

I know it should be possible since my windows pc does allow for just this scenario (Except it used the Line In instead of SPDIF In).

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I managed to do this by editing the Playback_to_Lineout.sh usage script so that the value after 'HPOUT2L Input 1' is AIF2RX1 and 'HPOUT2R Input 1' is AIF2RX2. I then ran that modified script and the SPDIF_record.sh usage script.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I did like youtomph, but put it all in one script. And for good measure, I added the possibility to use the equalizers on the Wolfson chip.

    The attached script takes an optional argument "eq". Run it without that argument and the sound goes straight from SPDIFin to LineOut.

     

    --

    Ragnar

    Attachments:
    https://community.element14.com/cfs-file/__key/communityserver-discussions-components-files/91/Listen_5F00_to_5F00_SPDIF.sh
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • eveready1010
    0 eveready1010 over 12 years ago in reply to e14 Contributor

    Yes!  That also worked like a charm!

     

    Thanks for the help!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi I tried the script, but when it is loaded on bootup, it only counts secounds and never stops.

    In case it makes a differents, I'm running Ubuntu MATE, on kernel 3.18

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi I tried the script, but when it is loaded on bootup, it only counts secounds and never stops.

    Which of the two scripts?

    There is nothing in my scripts that counts seconds, so that must be something else.

    What do you see on screen? Any error messages or other clues?

    In case it makes a differents, I'm running Ubuntu MATE, on kernel 3.18

    The scripts were made for the Wolfson card on Raspbian. Anything else is uncharted territory and anything could happen.

    --

    Ragnar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

                   It´s the init.d script. I deleted it and retried. Now I get this:

     

    ubuntu@UbuntuMATE:~$ sudo update-rc.d  wolfson-snd start 17 S . stop 17 0 1 6 .

    [sudo] password for ubuntu:

    insserv: Script wolfson-snd is broken: incomplete LSB comment.

    insserv: missing `Provides:' entry: please add.

    insserv: missing `Required-Start:' entry: please add even if empty.

    insserv: missing `Required-Stop:'  entry: please add even if empty.

    insserv: missing `Default-Start:'  entry: please add even if empty.

    insserv: missing `Default-Stop:'   entry: please add even if empty.

    insserv: Default-Start undefined, assuming empty start runlevel(s) for script `wolfson-snd'

    insserv: Default-Stop  undefined, assuming empty stop  runlevel(s) for script `wolfson-snd'

     

                    Should I reomove the #´s from the INIT INFO?

     

    ### BEGIN INIT INFO

        # Provides:          wolfson-snd

        # Required-Start:    $local_fs $remote_fs

        # Required-Stop:    $remote_fs

        # Default-Start:    S

        # Default-Stop:      0 1 6

        # Short-Description: Set Wolfson Audio Card SPDIF sampling rate and bit dep$

        # Description:       This script unmutes SPDIF In and Line Out and sets SPD$

        #                    It mutes SPDIF In and Line-Out on shutdown and reboot.$

        ### END INIT INFO

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    No, the # signs should be there.

    I think you have gotten junk characters into the script. It's common when you copy-paste from web sites.

    If you copy from this site, choose "expand source" and copy from there. Don't choose "view plain", it's known to introduce extra, invisible characters in some cases.

     

    Some of the mixer controls have changed names in the 3.18 drivers, change "SPDIF in" to "SPDIF In" on lines 76 and 88.

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Unit wolfson-snd.service has begun starting up.

    Apr 30 11:01:17 UbuntuMATE systemd[1660]: Failed at step EXEC spawning /etc/init.d/wolfson-snd: Exec format error

    -- Subject: Process /etc/init.d/wolfson-snd could not be executed

    -- Defined-By: systemd

    -- Support: http://lists.freedesktop.org/mailman/listinfo/systemd-devel

    --

    -- The process /etc/init.d/wolfson-snd could not be executed and failed.

    --

    -- The error number returned by this process is 8.

    Apr 30 11:01:17 UbuntuMATE systemd[1]: wolfson-snd.service: control process exited, code=exited status=203

    Apr 30 11:01:17 UbuntuMATE systemd[1]: Failed to start LSB: Set Wolfson Audio Card SPDIF sampling rate and bit depth..

    -- Subject: Unit wolfson-snd.service has failed

    -- Defined-By: systemd

    -- Support: http://lists.freedesktop.org/mailman/listinfo/systemd-devel

    --

    -- Unit wolfson-snd.service has failed.

    --

    -- The result is failed.

    Apr 30 11:01:17 UbuntuMATE systemd[1]: Unit wolfson-snd.service entered failed state.

    Apr 30 11:01:17 UbuntuMATE systemd[1]: wolfson-snd.service failed.

    Apr 30 11:01:17 UbuntuMATE polkitd(authority=local)[617]: Unregistered Authentication Agent for unix-process:1655:232095 (

    Apr 30 11:01:17 UbuntuMATE sudo[1645]: pam_unix(sudo:session): session closed for user root

     

    ubuntu@UbuntuMATE:~$ sudo chmod 755 /etc/init.d/wolfson-snd

    ubuntu@UbuntuMATE:~$ sudo /etc/init.d/wolfson-snd start

    [....] Starting wolfson-snd (via systemctl): wolfson-snd.serviceJob for wolfson-snd.service failed. See "systemctl status wolfson-snd.service" and "journalctl -xe" for details.

    failed!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Ok, I gave up. I´ll just use .desktop shortcuts for a little more convenience. I put one in the autostart folder, but it still doesn´t run automatically:

     

     

     

    GNU nano 2.2.6Datei: /etc/xdg/autostart/Setrate4816.desktop         

     

    [Desktop Entry]

    Type=Application

    Name=Setrate4816

    Exec=/usr/local/bin/SetRate48_16.sh

    Terminal=true

    X-MATE-Autostart-enabled=true

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eveready1010
    0 eveready1010 over 10 years ago in reply to e14 Contributor

    This script worked perfectly up until about a month ago, when the SD card would no longer write, so I was forced to rebuild the Wolfson Pi with the latest from Driver fixes and updates to kernel 3.18.16 and 4.0.5 but I am struggling with getting the script to work with the new build.  I have tried the script with the 4.1.19 and 4.4.6 build on the PiB with the Wolfson card, and also on the Pi2 with the Cirrus Card, but I get the same thing:

     

    $ wolfson-snd start

    [....] Setting up Wolfson Audio Card hw:0 192000 24...amixer: Cannot find the given element from control hw:0

     

    Then it just hangs.  So I CTRL-Z:

     

    ^Z
    [1]+  Stopped                 ./wolfson-snd start

     

    And then I looked in the /tmp folder, and there were a bunch of .wav files:

    wolfson-snd-01.wav

    wolfson-snd-02.wav

    ...

    All were exactly 44 bytes long.

     

    Plus the arecord process and the wolfson-snd process were still in memory and needed to be killed.

     

    It seems that there have been some changes between the original version and the current version of the driver, and/or alsa.

     

    It seems that the card does at least partially work, because I can play a wav file to the Line Out without issues.  The one thing that I noticed is that there are a lot of levels missing in the alsamixer application.  A bunch say "None" instead of having an adjustable volume or level control.  Not sure why this is that way.

     

    I have tried going through the script and running each command individually, and there are many anomalies.  Like some of the amixer commands complain that the control does not exist.  I tried running the amixer command to get all of the controls and output it to a file, which I then looked for an alternate or different but similarly named control.  It seemed I was partially successful at finding some but not all of the new control names.

     

    I am not sure what else to do.  I know this exact same card (WolfsonPi) was able to do what the script is designed to tell it to do, but now suddenly it no longer works.

     

    Any help or a point in the right direction would be appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to eveready1010

    Do you have the original sdcard? If so copy it byte for byte using the DD command to a new card..

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eveready1010
    0 eveready1010 over 10 years ago in reply to clem57

    I no longer have the original card, but I did save the scripts from it.

     

    Any other suggestions as to why the new driver or alsa seems to be different from the original design?  Also, I thought I had an original image from the Wolfson that I downloaded from element14 but that did not seem to help either, plus I don't know if it was in fact the original Wolfson img file.  It seems like the ability to listen to the SPDIF on the line out is no longer available in the newer release of the driver or os?

     

    Again, any help would be appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • eveready1010
    0 eveready1010 over 10 years ago in reply to clem57

    I no longer have the original card, but I did save the scripts from it.

     

    Any other suggestions as to why the new driver or alsa seems to be different from the original design?  Also, I thought I had an original image from the Wolfson that I downloaded from element14 but that did not seem to help either, plus I don't know if it was in fact the original Wolfson img file.  It seems like the ability to listen to the SPDIF on the line out is no longer available in the newer release of the driver or os?

     

    Again, any help would be appreciated.