Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver instability issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 3840 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver instability issue

e14 Contributor
e14 Contributor over 12 years ago

I've got the Wolfson Audio card running with an application that makes use of the Line-In and Line-Out ports. The Line-In port is _constantly_ read and to the Line-out port audio is written in parallel from time to time. Sampling rate is 48k. The kernel is compiled following the description here in this forum.

 

 

I now had the issue twice that the app hangs after about a day and a half. The second time I was able to collect the following info:

 

End of dmesg:

root@raspberrypi:/home/pi# dmesg | tail
 [135777.724427] arizona spi0.1: FLL1: Timed out waiting for lock
 [136377.676455] arizona spi0.1: FLL1: Timed out waiting for lock
 [136977.638482] arizona spi0.1: FLL1: Timed out waiting for lock
 [137577.600549] arizona spi0.1: FLL1: Timed out waiting for lock
 [138099.977529] arizona spi0.1: FLL1: Timed out waiting for lock
 [138777.524608] arizona spi0.1: FLL1: Timed out waiting for lock
 [139377.496589] arizona spi0.1: FLL1: Timed out waiting for lock
 [139977.448573] arizona spi0.1: FLL1: Timed out waiting for lock
 [139977.522931] ERROR: 4096 KiB atomic DMA coherent pool is too small!
 [139977.522931] Please increase it with coherent_pool= kernel parameter!

 

 

The app hangs. After kill -9 any attempt to restart fails with the following message from the app:

 

*** ERROR: snd_pcm_start failed (unrecoverable error): Cannot allocate memory
 *** ERROR: Start capture failed

 

Here is the end of the corresponding strace of an app start attempt:

 

stat64("/usr/share/alsa/alsa.conf", {st_mode=S_IFREG|0644, st_size=9184, ...}) = 0
 open("/dev/snd/controlC0", O_RDONLY|O_CLOEXEC) = 5
 fcntl64(5, F_SETFD, FD_CLOEXEC)         = 0
 ioctl(5, UI_DEV_CREATE, 0xbef492cc)     = 0
 close(5)                                = 0
 open("/dev/snd/controlC0", O_RDWR|O_CLOEXEC) = 5
 fcntl64(5, F_SETFD, FD_CLOEXEC)         = 0
 ioctl(5, USBDEVFS_CONTROL or USBDEVFS_CONTROL32, 0xbef4946c) = 0
 ioctl(5, 0x40045532, 0xbef494a4)        = 0
 open("/dev/snd/pcmC0D0c", O_RDWR|O_NONBLOCK|O_CLOEXEC) = 6
 fcntl64(6, F_SETFD, FD_CLOEXEC)         = 0
 close(5)                                = 0
 ioctl(6, AGPIOC_ACQUIRE or APM_IOC_STANDBY, 0xbef492e8) = 0
 fcntl64(6, F_GETFL)                     = 0x802 (flags O_RDWR|O_NONBLOCK)
 ioctl(6, AGPIOC_INFO, 0xbef492dc)       = 0
 clock_gettime(CLOCK_MONOTONIC, {172144, 75851672}) = 0
 ioctl(6, AGPIOC_SETUP, 0xbef492e4)      = 0
 mmap2(NULL, 4096, PROT_READ, MAP_SHARED, 6, 0x80000) = -1 ENXIO (No such device or address)
 ioctl(6, 0xc0844123, 0xbef49408)        = 0
 fcntl64(6, F_GETFL)                     = 0x802 (flags O_RDWR|O_NONBLOCK)
 fcntl64(6, F_SETFL, O_RDWR)             = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4110, 0x1935718)         = 0
 ioctl(6, 0xc25c4111, 0x1935718)         = 0
 ioctl(6, 0xc0844123, 0x1935bb8)         = 0
 ioctl(6, 0xc0684113, 0xbef496d4)        = 0
 ioctl(6, 0x4140, 0xb69d5000)            = 0
 ioctl(6, 0xc0844123, 0x1935bb8)         = 0
 ioctl(6, 0xc0684113, 0x19353e0)         = 0
 ioctl(6, 0x4140, 0xb69d5000)            = 0
 ioctl(6, 0xc0844123, 0x1935bb8)         = 0
 ioctl(6, 0xc0844123, 0x1935bb8)         = 0
 ioctl(6, 0x4142, 0x1935bb8)             = -1 ENOMEM (Cannot allocate memory)
 write(2, "*** ERROR: snd_pcm_start failed "..., 55*** ERROR: snd_pcm_start failed (unrecoverable error): ) = 55
 write(2, "Cannot allocate memory", 22Cannot allocate memory)  = 22
 write(2, "\n", 1
 )                       = 1
 write(2, "*** ERROR: Start capture failed", 31*** ERROR: Start capture failed) = 31
 write(2, "\n", 1
 )                       = 1
 ioctl(6, 0x4143, 0xb69d5000)            = 0
 ioctl(6, 0x4112, 0xf5519900)            = 0
 close(6)                                = 0
 write(2, "*** ERROR: Could not open audio "..., 53*** ERROR: Could not open audio device for receiver ") = 53
 write(2, "Rx1", 3Rx1)                      = 3
 write(2, "\"\n", 2"
 )                     = 2
 close(4)                                = 0
 brk(0x1955000)                          = 0x1955000
 brk(0x1947000)                          = 0x1947000
 write(2, "*** ERROR: Could not initialize "..., 36*** ERROR: Could not initialize RX ") = 36
 write(2, "Rx1", 3Rx1)                      = 3
 write(2, "\"\n", 2"
 )                     = 2
 write(2, "*** ERROR: Could not initialize "..., 46*** ERROR: Could not initialize Logic object ") = 46
 write(2, "RepeaterLogic", 13RepeaterLogic)           = 13
 write(2, "\". Skipping...\n", 15". Skipping...
 )       = 15
 write(2, "*** ERROR: No logics available. "..., 47*** ERROR: No logics available. Bailing out...
 ) = 47
 exit_group(1)                           = ?

 

BTW, the app is supposed to run _for-ever_ reading and processing audio... running for two years without restart is common for users of this app on x86 hardware.

 

Is there any driver update on the way that could fix this (and allow lower sampling rates on the analogue input)?

Thanks?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Does anyone know if there is still somebody working on this issue?

     

    I also ran into the "ERROR: 4096 KiB atomic DMA coherent pool is too small!" error using a 3.16.5 kernel on a Raspberry Compute Module. It came up unexpectedly after a few minutes of playing around with aplay and gst-launch. First the system froze for about 2 minutes (but I could still ping it), then it came back to life with the error, plus I/O errors on the SD card interface because the system was in the middle of writing some file when the error occurred. File system was corrupted after a power cycle...

     

    Today, I checked again with kernel 3.19.0 (revision f589118 from https://github.com/raspberrypi/linux.git) and tried something similar to what Paul Roe has done in post #10, but with aplay instead of arecord. Apparently there were some changes applied to the I2S driver, so I was hoping for better results than with 3.16.5, but I got disappointed.

     

    Here is what I've tried with a simple one second long stereo file at 44.1 kHz:

     

    $ for i in $(seq 10000); do aplay 1sec.wav || break; echo $(date) $i; done

    Playing WAVE '1sec.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo

    Fri Feb 13 08:53:17 UTC 2015 1

    ....

    This went on for about 20 minutes, then after a bit more than 900 iterations the loop broke.

     

    Attempting to play the .wav with aplay yielded an error after ten seconds ("aplay: pcm_write:1947: write error: Input/output error").

    Attempting to cat some random file not already in fscache also yielded an I/O error (maybe trying to load the cat executable already gave the error, not sure).

     

    To my surprise, there was no atomic-DMA-coherent-pool-error, but found this in the kernel log after these actions:

    [ 1732.219441] mmc0: Timeout waiting for hardware interrupt.

    [ 1732.225168] mmcblk0: error -110 transferring data, sector 3013168, nr 32, cmd response 0x900, card status 0xb00

    [ 1732.236730] mmcblk0: retrying using single block read

    [ 1772.279443] mmc0: Timeout waiting for hardware interrupt.

    [ 1772.285206] mmcblk0: error -110 transferring data, sector 3707576, nr 16, cmd response 0x900, card status 0xd00

    [ 1772.296995] blk_update_request: I/O error, dev mmcblk0, sector 3707576

    [ 1772.303841] blk_update_request: I/O error, dev mmcblk0, sector 3707584

    [ 1772.311732] Aborting journal on device mmcblk0p7-8.

    [ 1782.319444] mmc0: Timeout waiting for hardware interrupt.

    [ 1782.325167] mmcblk0: error -110 transferring data, sector 3301472, nr 8, cmd response 0x900, card status 0xb00

    [ 1782.336796] mmcblk0: retrying using single block read

    [ 1792.359440] mmc0: Timeout waiting for hardware interrupt.

    [ 1792.365216] mmcblk0: error -110 transferring data, sector 3706880, nr 8, cmd response 0x900, card status 0xd00

    [ 1792.376864] blk_update_request: I/O error, dev mmcblk0, sector 3706880

    [ 1792.383702] Buffer I/O error on dev mmcblk0p7, logical block 131072, lost sync page write

    [ 1792.393305] JBD2: Error -5 detected when updating journal superblock for mmcblk0p7-8.

     

    Well, the DMA-related error message was removed as part of a bigger change in 36d0fd2, so it cannot show up anymore.

     

    Needless to say, attempting to cleanly shut down via shutdown -r now yielded more errors. I power-cycled the system after several minutes of waiting. There was no file system corruption this time (system booted, fsck.ext4 -v -n -f reported no errors), probably because there was no coincidental writing in the background when the I/O errors started to show up.

     

    So, the original problem seems to persist: playing audio over I2S kills the system and may lead to file system corruption even in the latest kernel version.

    Is there anyone who is working on this problem?

     

    By the way, the patch from post #12 does not apply to the latest kernel anymore. As it contains the work "hack" many times, I am also not so sure that it should be used in production anyway. I didn't try it on older kernels.

     

     

    Maybe unrelated, but I also found this in the kernel log:

    [  602.269309] bcm2708_fb_blank(1) returns=1 p[1]=0x0

    That's the video driver speaking here (linux/drivers/video/bcm2708_fb.c).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Did you compile Kernel 3.19 with cirrus/wolfson drivers? When I compiled the driver I only got 3.18. https://github.com/CirrusLogic/rpi-linux/wiki/Building-the-code

    How did you do it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Did you compile Kernel 3.19 with cirrus/wolfson drivers? When I compiled the driver I only got 3.18. https://github.com/CirrusLogic/rpi-linux/wiki/Building-the-code

    How did you do it?