Raspberry Pi Forum Raspi and AWUS036H setup
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 683 subscribers
  • Views 924 views
  • Users 0 members are here
Related

Raspi and AWUS036H setup

Former Member
Former Member over 11 years ago

My eyes are bleery. i've checked the forums and Googled for hours now, but still can't get my Raspi to use my USB WiFi adaptor.

 

Am using raspberrypi 3.10.25+, fully updated.

 

i presently have access to the Raspi through an Ethernet connection, my home computer, ssh and vinagre. i almost feel like a hacker. Almost all of the forum posts in Google have to do with wardriving - lol.

 

i just want to be able to set up the Raspi and NOT have it use the Ethernet connection/cable when it boots up so we can go on to the next step of using it to measure temperatures on our solar hot water heater setup.

  • Sign in to reply
  • Cancel
Parents
  • element14jamie
    0 element14jamie over 11 years ago

    Hello frazelle09,

    Welcome to element14 Community, I will move this over to the Raspberry Pi area of the community as it is a better fit. If at anytime you feel that there is an issue with the product please hover over my avatar to get my email and contact me directly so I can further assist.

     

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to element14jamie

    Hi Frederick,

     

    The pasting still looks a little messed, I think the content of the two files looks a little mixed. Once you have pasted the content you can highlight it, and select the icon that looks like " >> " on the editor toolbar, and select "Syntax Highlighting" and then select "Plain".

    Then it looks like this.

     

    Anyway, the config looks a bit different to the one in the links earlier, but I don't know if that is the cause or not (your config may be fine, it's just I've only used the method in the earlier links).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago in reply to element14jamie

    Hi Frederick,

     

    The pasting still looks a little messed, I think the content of the two files looks a little mixed. Once you have pasted the content you can highlight it, and select the icon that looks like " >> " on the editor toolbar, and select "Syntax Highlighting" and then select "Plain".

    Then it looks like this.

     

    Anyway, the config looks a bit different to the one in the links earlier, but I don't know if that is the cause or not (your config may be fine, it's just I've only used the method in the earlier links).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to shabaz

    Thanks, shabaz for your kind and rapid reply.  We'll try again to insert the info...

     

         At this point iwconfig gives...

    iwconfig
    wlan0     IEEE 802.11bg  ESSID:off/any 
              Mode:Managed  Access Point: Not-Associated   Tx-Power=20 dBm  
              Retry  long limit:7   RTS thr:off   Fragment thr:off
              Encryption key:off
              Power Management:off
             
    lo        no wireless extensions.

    eth0      no wireless extensions.

    lsmod produces...

     

    lsmod
    Module                  Size  Used by
    bnep                   10792  2
    rfcomm                 32939  0
    bluetooth             221259  10 bnep,rfcomm
    snd_bcm2835            16165  0
    arc4                    1683  2
    snd_soc_bcm2708_i2s     5474  0
    regmap_mmio             2806  1 snd_soc_bcm2708_i2s
    rtl8187                51399  0
    snd_soc_core          131268  1 snd_soc_bcm2708_i2s
    regmap_spi              1897  1 snd_soc_core
    snd_pcm                81593  2 snd_bcm2835,snd_soc_core
    snd_page_alloc          5156  1 snd_pcm
    mac80211              315594  1 rtl8187
    regmap_i2c              1645  1 snd_soc_core
    snd_compress            8076  1 snd_soc_core
    snd_seq                53769  0
    snd_timer              20133  2 snd_pcm,snd_seq
    snd_seq_device          6473  1 snd_seq
    cfg80211              209273  2 mac80211,rtl8187
    rfkill                 19138  3 cfg80211,bluetooth
    eeprom_93cx6            2975  1 rtl8187
    leds_gpio               2059  0
    led_class               3688  2 leds_gpio,rtl8187
    snd                    61291  7 snd_bcm2835,snd_soc_core,snd_timer,snd_pcm,snd_seq,snd_seq_device,snd_compress
    root@raspberrypi:/home/pi#

    /etc/network/interfaces is...

     

    auto lo

    iface lo inet loopback
    iface eth0 inet dhcp

    #allow-hotplug wlan0
    #iface wlan0 inet manual
    #wpa-roam /etc/wpa_supplicant/wpa_supplicant.conf
    #iface default inet dhcp

    auto wlan0
    allow-hotplug wlan0
    iface wlan0 inet dhcp
    wpa-ssid xxxxxxxxx
    wpa-psk xxxxxxx

    and /etc/wpa_supplicant/wpa_supplicant is...

     

    ctrl_interface=DIR=/var/run/wpa_supplicant update_config=1

    network={
            ssid="xxxxxxxxxx"
            psk="xxxxxxxxx"
            proto=RSN
            key_mgmt=WPA-PSK
            pairwise=CCMP
            auth_alg=OPEN
    }

    Hopefully this looks a little better and we can proceed from here.

     

    Have a great afternoon!  image