Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum NEW TO RPI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 705 subscribers
  • Views 970 views
  • Users 0 members are here
  • help
  • raspberry_pi
  • newbie
  • advice
Related

NEW TO RPI

e14 Contributor
e14 Contributor over 12 years ago

hey im new to rasberry pi and im stuck on an idea for it  i mean im not sure  what do i got it up and running on raspbain  OS  is there a way to change it after or no? and how do you use scratch and also what can you attach to it  also is there away to add more power i.e RAM other then usb stick and is there a work around for flash player? and does any have beginner level of project i could try out?

  • Sign in to reply
  • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago

    I've heard that The MagPi magazine is a good source for RasPi project ideas: http://www.themagpi.com/

     

    There's no way to add RAM unless somebody offers it on an SD card or USB module.  You can change OS by programming multiple SD cards with different OSes and plugging in the one you want to boot.  I think Noobs can do this on a single SD card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to johnbeetem

    thanks  and do you know anyway to connect the rpi to  to bread board  to control LEDS i ve been searching for a guide or a tutorial on how to, to get me use to working   with the pi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    for breadboard look at this http://canada.newark.com/adafruit-industries/914/pi-cobbler-breakout-kit-raspberry/dp/44W3497

     

    for general PI kit look here: http://canada.newark.com/raspberry-pi-accessories?rd=raspberry+pi&catalogId=15003&langId=1&storeId=10196

     

    and then from there you can look to the community and also Ada-fruit and other resources for great ideas including what John has already pointed you to

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to e14 Contributor

    There's a bunch of RasPi tutorials and projects at Adafruit: https://learn.adafruit.com/category/raspberry-pi

     

    This one is probably the most helpful to get started: https://learn.adafruit.com/raspberry-pi-e-mail-notifier-using-leds

     

    The best reference I've seen on GPIOs is the RasPi Hardware Wiki: http://elinux.org/RPi_Low-level_peripherals

    This page includes both hardware and software.  Basically, all you need hardware-wise is a single RasPi GPIO connected to a 200 to 1K Ohm or series resistor to limit current connected to the anode of the LED, with the cathode of the LED connected back to RasPi's ground.

     

    Be very careful when playing with the RasPi GPIOs because if you short a 5V pin to 3.3V or a GPIO you can permanently damage RasPi.  I stick short pieces of wire insulation over those pins so I don't accidentally touch them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    You can use the GPIO ports. (aka the prongs on your RPI). Here is a diagram describing the RPI GPIO Ports.

    Model A

    Raspberry-Pi-GPIO-Layout-Revision-1.png

    Model B

    Raspberry-Pi-GPIO-Layout-Revision-2.png