Raspberry Pi Forum Wolfson audio card + Jasper ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 2 answers
  • Subscribers 687 subscribers
  • Views 3500 views
  • Users 0 members are here
  • wolfson
  • jasper
  • audio
  • alsa
  • voice
  • raspberry_pi
  • raspberrypi
  • raspeberry_pi_accessories
Related

Wolfson audio card + Jasper ?

fvan
fvan over 11 years ago

Hi,

 

has anyone been able to get Jasper (Jasper | Control everything with your voice ) to work with the Wolfson audio card ?

 

I tried getting it to work with two different approaches and ended up with the same result (which is something good I suppose).

  • Took the Wolfson image and manually installed Jasper software
  • Took the Jasper image and manually installed Wolfson drivers/kernel

 

Jasper is working via the command line, but when trying to use voice control, I get some (Alsa related?) errors.

 

Expression 'PaAlsaStream_Configure( stream, inputParameters, outputParameters, sampleRate, framesPerBuffer, &inputLatency, &outputLatency, &hostBufferSizeMode )' failed in 'src/hostapi/alsa/pa_linux_alsa.c', line: 2762
Expression 'r' failed in 'src/hostapi/alsa/pa_linux_alsa.c', line: 2013
Expression 'PaAlsaStreamComponent_FinishConfigure( &self->capture, hwParamsCapture, inParams, self->primeBuffers, realSr, inputLatency )' failed in 'src/hostapi/alsa/pa_linux_alsa.c', line: 2650

 

Full log attached.

 

Thanks!

Frederick

Attachments:
jasper_log.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • bantammenace
    0 bantammenace over 10 years ago

    I've successfully used a Wolfson Audio Card with Gerrelt's (Truehl) Squeezeplug Logitech Media Server on a RPi B since it was first included in the Squeezeplug image.

    Recently and primarily using Ragnar's (excellent) instructions for setting up the WAC I have the Subsonic open-source web-based media streamer and jukebox working on another RPi B with a WAC.

    Now I am trying to get a RPI B to work with the WAC and Jasper. Unfortunately after many, many, many hours of trying and many fresh attempts I just cannot get it to install/run successfully. I suspect that not all the links in the instructions are pointing to where they should be.

    I would really appreciate it if someone could provide a working image that I could download. I just love the idea of using the on board microphones to pause/mute my music and I want top try and avoid having to go down the external USB mic route

    I will also post this on the Jasper forum and the Raspberry Pi  forum and will let all three forums if anyone is kind enough to provide a copy of their fully working image. Before anyone does I would probably recommend that they run populate.py again and enter through all the stages without entering their personal details.

    Certainly it would help CFC Farnell to sell their remaining stock of WACs which otherwise I would imagine would be languishing on the shelves of a warehouse somewhere until the decision was taken to send them to the tip,

    Today they are showing as having 2680 in stock which at the current price of £16.50 UK pounds is £44,220 UK pounds. Perhaps CPC Farnell could pay Ragnar something to create an image ?

    Thanks for reading,

    Thanks in advance

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bantammenace
    0 bantammenace over 10 years ago

    I've successfully used a Wolfson Audio Card with Gerrelt's (Truehl) Squeezeplug Logitech Media Server on a RPi B since it was first included in the Squeezeplug image.

    Recently and primarily using Ragnar's (excellent) instructions for setting up the WAC I have the Subsonic open-source web-based media streamer and jukebox working on another RPi B with a WAC.

    Now I am trying to get a RPI B to work with the WAC and Jasper. Unfortunately after many, many, many hours of trying and many fresh attempts I just cannot get it to install/run successfully. I suspect that not all the links in the instructions are pointing to where they should be.

    I would really appreciate it if someone could provide a working image that I could download. I just love the idea of using the on board microphones to pause/mute my music and I want top try and avoid having to go down the external USB mic route

    I will also post this on the Jasper forum and the Raspberry Pi  forum and will let all three forums if anyone is kind enough to provide a copy of their fully working image. Before anyone does I would probably recommend that they run populate.py again and enter through all the stages without entering their personal details.

    Certainly it would help CFC Farnell to sell their remaining stock of WACs which otherwise I would imagine would be languishing on the shelves of a warehouse somewhere until the decision was taken to send them to the tip,

    Today they are showing as having 2680 in stock which at the current price of £16.50 UK pounds is £44,220 UK pounds. Perhaps CPC Farnell could pay Ragnar something to create an image ?

    Thanks for reading,

    Thanks in advance

    Kind regards