Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Using GPIO4 and GPIO3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 699 subscribers
  • Views 686 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Using GPIO4 and GPIO3

e14 Contributor
e14 Contributor over 12 years ago

Hi

 

In my project, I would like to use pins GPIO4 and GPIO3 (on the wolfson card) to attach and control 2 leds. I would like to use these to give some feedback to the user about my program while no screen is attached.

 

Is this possible? If so, how to swtich on/off these pins? Can I use the stock RPI.GPIO python module using the following code:

 

GPIO.output(15, True) #for  gpio3

GPIO.output(16, True) #for  gpio4

 

Best

Dieter

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Your best option for just 2 LEDs is to use GPIO14/15, the UART lines.

    Disable the serial boot logging and the default serial console and you can use these two lines as general I/O pins.

     

    Edit boot commandline:

    sudo nano /boot/cmdline.txt

    Remove "console=ttyAMA0,115200 kgdboc=ttyAMA0,115200"

     

    Edit /etc/inittab:

    sudo nano etc/inttab

    Comment the line "2:23:respawn:/sbin/getty -L ttyAMA0 115200 vt100"

    by adding a hash '#' at the start of the line.

     

    Reboot and GPIO14 & GPIO15 (BCM nmubering) are available as I/O lines.

     

    Tutorial here

     

    I connected a pair of LEDs to the J8 header on my Wolfson card yesterday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for this.

     

    Does this mean that gpio3 and gpio4 are not simpely passed through from the Pi? Are they connected to the chipset of the wolfson card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for this.

     

    Does this mean that gpio3 and gpio4 are not simpely passed through from the Pi? Are they connected to the chipset of the wolfson card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I don't think GPIO3 & GPIO4 on the Expand Header are RasPi GPIO lines IDs.

    WAC.GPIO3 is shown connected to Pi P1.22 (Pi.GPIO25)

    WAC.GPIO4 does not seem to connect to the Pi GPIO.

    Both are presumably used by the board and not available to you for general IO.

     

    See the schematic

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer