Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry PI  (B) + NXP Explore NFC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 708 subscribers
  • Views 1115 views
  • Users 0 members are here
  • raspberry_pi
  • nfc
  • explorenfc
Related

Raspberry PI  (B) + NXP Explore NFC

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

Please help!!

 

I have purchased a Raspberry Pi (B) and a NXP Explore NFC board, I need to use them to send file from Raspberry to NFC enabled phone.

I have tried the demo/sample code but no luck, it just cannot detect my NFC enabled phone (Samsung Note II).

Can someone help?

 

regards

 

 

pi@raspberrypi ~/NFC/P2P-SNEP_clientPUT $ sudo ./Snep_client

Enter: piBoardRev

piboardRev: Revision string: 000d

, board revision: 2

OK: phbalReg_R_Pi_spi_Init

wId: 109

spiFD: 0

spiMode: 0

spiBPW: 8

spiDelay: 0

spiSpeed: 1e8480 2000000

Enter: phbalReg_R_Pi_spi_OpenPort

Chip version: 82

phpalI14443p3a_Sw_Init

phpalI14443p4a_Sw_Init

phpalI14443p3b_Sw_Init

phpalFelica_Sw_Init

phpalI18092mPI_Sw_Init

phacDiscLoop_Sw_Init

phhalHw_FieldReset

DiscLoopInit

DiscLoopDemo

Pooling: 5

Pooling: 4

Pooling: 3

Pooling: 2

Pooling: 1

Pooling: 5

Pooling: 4

Pooling: 3

Pooling: 2

Pooling: 1

Pooling: 5

Pooling: 4

Pooling: 3

Pooling: 2

Pooling: 1

Pooling: 5

Pooling: 4

Pooling: 3

Pooling: 2

Pooling: 1

Pooling: 5

Pooling: 4

Pooling: 3

Pooling: 2

Pooling: 1

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I went back to project one, got that working then moved on to project two, then modified the NDEF message to pass the data I needed to pass to the device. I did attempt to add database access to make the NDEF message dynamic, but whilst I could make it work outside of the project, once I tried to implement it in to the project I had no luck, spent about 12 solid hours on it and got nowhere. In the end I just modified the NDEF message to point to an external URL and used PHP to take care of the dynamic information. It is a shame I was unable to apply this in C, I may try again in the future.

     

    I'll check out the link, thanks.

     

    @ OP, try starting out with project one, and going from there. Also get hold of a standard MiFARE NFC tag and see if it can see that, and maybe the card that comes with the dev pack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I went back to project one, got that working then moved on to project two, then modified the NDEF message to pass the data I needed to pass to the device. I did attempt to add database access to make the NDEF message dynamic, but whilst I could make it work outside of the project, once I tried to implement it in to the project I had no luck, spent about 12 solid hours on it and got nowhere. In the end I just modified the NDEF message to point to an external URL and used PHP to take care of the dynamic information. It is a shame I was unable to apply this in C, I may try again in the future.

     

    I'll check out the link, thanks.

     

    @ OP, try starting out with project one, and going from there. Also get hold of a standard MiFARE NFC tag and see if it can see that, and maybe the card that comes with the dev pack.