Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum can i build an led cube and to control it with raspberry
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 13 answers
  • Subscribers 710 subscribers
  • Views 3156 views
  • Users 0 members are here
  • raspberry_pi
Related

can i build an led cube and to control it with raspberry

e14 Contributor
e14 Contributor over 12 years ago

images?q=tbn:ANd9GcRqC9Gqane0sozu4TkkAGalkeFBBh-Np5H5fJ2tAw1eUVDPK-GNJLwm7AHello im wondering if is there any possibility to use raspberry as a controller for the led cube ?

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    for smooth operation though i'm not sure if the PI will be up to the task, having it as a master and sending the pattern requests to the Arduino is good. I have not yet seen a PI do this. Not saying it cant be done but to be honest, a PI is not the best choice for hardware control of this nature. An Arduino or similar (MSP430, TivaC etc) is much more adept.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to Robert Peter Oakes

    Like this http://jacksonliam.blogspot.ca/2012/06/arduino-and-raspberry-pi-talking-over.html

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to Robert Peter Oakes

    better link here with reasons http://www.raspberrypi.org/forums/viewtopic.php?f=38&t=10120

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to Robert Peter Oakes

    better link here with reasons http://www.raspberrypi.org/forums/viewtopic.php?f=38&t=10120

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • kidiccurus
    0 kidiccurus over 12 years ago in reply to Robert Peter Oakes

    Or just skip the pi and go straight to 'duino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to kidiccurus

    To make  a decent LED cube you need to get away from weedy little processors or RP with it's lack of IO and poor real time perfromance.

     

    This guy shows you how do it right http://www.hownottoengineer.com/projects/rgb-led-cube.html

    (And lot's of good explanation.)

     

    If I were doing it I would use an FPGA (which would get rid of the LED driver chips) but that's because I use them all the time so I have all the tools.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 12 years ago in reply to michaelkellett

    You don't necessarily need a driver chip with an arduino. For a 4x4x6 cube I am working on the only io expansion I am using is a single Johnson counter. This is using an arduino Leonardo.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to kidiccurus

    How will you get any power into your LEDs without drivers - you have 96 LEDs (which is a lot less than the 512 for an 8 x 8 x 8) cube but the maximum total current you can put out is less than 200mA  which won't be very bright. (Perhaps I'm missing something - can you post a sketch of your ciruit ?)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to michaelkellett

    that's total for the chip too, you are limited also to 20mA per pin, absolute max being 40mA but not recommended and that would also be dropping a lot of volts in the chip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to michaelkellett

    Micheal, although you would obviously have the number of pins available on an FPGA how would you handle the drive current ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to Problemchild

    I'd still need some power devices for a big display or  abright one but:

     

    The Lattice ECP2 in 208 pin TQFP package can do a maximum average IO current of 146 x 8 = 1168mA on 146 pins. You can't use all the pins for LEDs so over, say, the 96 pins of Samuel's cube it can do 12mA per LED continuous, no multiplexing required.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to michaelkellett

    can the FPGA handle the overall power dissipation, there is always a current per pin but also a total current per silicon chip with most often is not the sum of all or even most of the pins

     

    btw, typical LEDs require 20mA for full intensity, as you are multiplexing the pins (There not on continually ) then this current needs to go up proportionately, so if your at a 50% duty cycle, you need 40mA, 25%=80mA etc

     

    if you don't account for this then the typical result is un even brightness as the number of LEDs change over the pattern or they are quite dim all the time. just look at how a 7segment display works.

     

    yes you can get away with it to a certain extent (Small number of leds ) but it will bite you as your cube grows in size 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rew
    0 rew over 12 years ago in reply to Robert Peter Oakes

    Peter,
    Your concern about the total current (might be per VCC pin or per package) is valid.

     

    But about the current: I've built several "multiplexing" led projects over the last few years. Because of the risk of blowing up the leds should the software fail, I always build my prototype with the currentlimit set "below 20mA", intending to up the current when I'm done....

     

    I always end up with: "this looks just great like this, no need to increase the current!". Leds, these days, are simply bright enough at 1/8 multiplexing....

     

    I don't understand what you're saying about the brightness being uneven. If you put the current-limit-resistors in the right place, you'll be driving a column (A plane in the cube) with a power-transistor, and you have all diodes in this plane connected to a driver/one of the FPGA pins through a resistor.


    Michael was saying he wouldn't use a shift-register to drive the row-lines, because he can easily find 64 (for 8x8)  or 81 (for 9x9) row-lines on his FPGA. Nobody is saying you can get around those. Nobody should put current-limit resistors in the column drivers, as that creates brightness differences depending on the number of leds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to rew

    and that is where I was thinking the issue may be, thanks for clarifying, I have never built a cube yet, maybe some time but not yet.

     

    I have built plenty of multiplexed light displays in my time but built to the end game light requirements that where usually in the 10's of amps per channel (Fair ground rides like ferris wheels etc consume hundreds of amps before they went to LED lighting and 110V dc too)

     

    as you say though, at the end of the day if it looks good then that's good enough, no point in over engineering if you dont need to