Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is it possible to create a command line program?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 692 subscribers
  • Views 547 views
  • Users 0 members are here
  • raspberry_pi
Related

Is it possible to create a command line program?

Former Member
Former Member over 11 years ago

I am wondering if it is possible to create a program on the on the command line of the raspberry pi, like you would tell it to run a program and then it asks for you to provide an input. Is that possible?

  • Sign in to reply
  • Cancel
Parents
  • vish
    0 vish over 11 years ago

    If you want to call a program from your program( in C ) you can try these,

         system() - this will the command you specifies as argument and returns once that program is completed.

              Ex : system( "ls" );

         popen() - this can be used when you want to read the output of the executed program or input any options to the program but not both. Its much like you are dealing with files. Try 'man popen' from your command terminal for more info.

         execl() - these can also be used for starting an external program. Try 'man exec' for complete range of options.

    If you are looking to implement command line args in your C-program, you can find a good tutorial here - Anatomy of command line arguments in Linux

     

    If you are using python, check this : Python os.popen() Method

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • vish
    0 vish over 11 years ago

    If you want to call a program from your program( in C ) you can try these,

         system() - this will the command you specifies as argument and returns once that program is completed.

              Ex : system( "ls" );

         popen() - this can be used when you want to read the output of the executed program or input any options to the program but not both. Its much like you are dealing with files. Try 'man popen' from your command terminal for more info.

         execl() - these can also be used for starting an external program. Try 'man exec' for complete range of options.

    If you are looking to implement command line args in your C-program, you can find a good tutorial here - Anatomy of command line arguments in Linux

     

    If you are using python, check this : Python os.popen() Method

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
No Data