I have 12V Solenoid(Makeblock DC Frame Type Solenoid HCNE1-0530) and I want to control it using Piface, can this be done entirely using Piface ? or additional component will be require ?. circuit arrangement will be helpful
I have 12V Solenoid(Makeblock DC Frame Type Solenoid HCNE1-0530) and I want to control it using Piface, can this be done entirely using Piface ? or additional component will be require ?. circuit arrangement will be helpful
NVM, still can't dl images.
I would use a TLP351 logic optocoupler for my first stage. Output is CMOS push-pull totem pole. This is how I would get from logic voltage to solenoid voltage.
I would follow with a complementary-symmetry bipolar stage. NPN pull up, PNP pull down, bases bussed and connected to the output of the optocoupler. Emmiters bussed and connected to the load, far side of load to (solenoid)V-. Collectors go to respective sides of the solenoid supply. NPN energizes coil, PNP catches spikes.
I would simulate the stuffing out of this using SPICE before I attempted to assemble this, for you have little reason to trust me, or authority (not that I represent authority) generally. Try and measure the inductance of your coil so you can input it to SPICE.
Use Qs rated for at least a coupla amperes, we like to employ design-margin, esp. in one-offs.
what is SPICE ?
also I bought MOSFET Power Control Kit(https://www.sparkfun.com/products/10256) and successfully able to operate solenoid using piface digital output pin. but it is overheating now :-(
Spice is a "golden-oldie" electronic circuit simulator. I remember working with it in the 1980's. and even then it was an "old" program. Nowadays there are GUI frontends, but the calculations are still done mostly with the "old code".
Your mosfet is about 0.05 ohms. So at 1A (you look up and report back what your solenoid actually uses! it uses even less, 0.45A) you would get a voltage drop of about 0.05V. This would, at 1A generate about 50mW of power. This is so very little that it is hard to measure. So if it is overheating, there is something wrong. Show us your circuit (draw a circuit diagram of how you WANTED to connect things. Then also show us a picture of your actual build!).
Now for solenoids, the problem is that the solenoid will generate a voltage spike when it is turned off. If you turn it off often, that can cause heating. The mosfet is specified to tolerate a bit of misuse (*) in this area, but it is possible that you are exceeding the "a bit" part.... :-)
Still, the freewheeling diode may be a good idea anyway: it can't hurt (if connected right side up).
(*) Many electronics engineers will say you HAVE to provide a freewheeling diode, but this mosfet is SPECIFIED to work without one, as long as certain requirements are met.
as internal resistance of your device is 27ohms it may not heat up mosfet... if mosfet heating up slowly then its fine put some heatsink..
sorry for confusion, it is not mosfet heating up, it is a Solenoid which is overheating.
sorry for confusion, it is not mosfet heating up, it is a Solenoid which is overheating.
I will assemble my circuit and post picture soon
The solenoid is specified to have a resistance of 27 ohms. That results in 0.45A of current. That should come to about 5.4W.
It should get noticably warm with that. I'm not sure if the solenoid is specified to be "continuously on", or if it is meant to be on for only short periods. Does it really overheat (and break?) , or is it just that you find that it is getting too hot to touch?
I did not run it until it breaks, but it is getting too hot to touch. also I notice that piface Pin LED slightly remain lit up even after supplying signal zero.
if your leaving the solenoid energized then it will be drawing 500mA at 12V meaning 6W of heat dissipation
if it is excessively hot then I would suspect it is not 12V 500mA or requiring a lower holding voltage as described above
Any chance you can post a link or similar to the solenoid.
Many require the plunger to be in to reduce the energy loss, some are AC, some are DC and they aren't the same.
The other thing to try is .... connect it across 12v and does it get hot after 10-30 secs.
If it does then it isn't designed for continuous operation and you need to be able to reduce the current.
mark
The link to the solenoid is in the opening post. Makeblock DC Frame Type Solenoid HCNE1-0530
The link to the solenoid is in the opening post. Makeblock DC Frame Type Solenoid HCNE1-0530
sorry I missed that.
However the link provides a lot of poor translation and the temperature rise is less English and more gibberish.
The reference to ED 25% leads me to believe its not highly rated,
That is the power can only be applied for 25% of the time but it doesn't give a maximum time.
so 30 secs ON and 90 secs OFF is 25% duty cycle.
I suspect this is why there is a heating effect noted by the OP..
Mark
Ah, yes, the ED is probably the max allowable on-time-percentage.
Your "thirty seconds" sounds about right (and on the safe side). So after having it on for (max) 30 seconds, it needs to be off for 90 seconds (or 3 times the time it was on).
Hmm. Doing a power-calculation means that it can dissipate about 25% of the power it produces at 12V. Thus if your application allows it, you might be able to pulse it at 12V to get it to move, and then hold it at 6V....
And at 50g I doubt it will be much use to the OP.
It may work but there will be some experimenting required ....
Mark
As the magnetic force drops quadratically, I think it is quite possible that if it provides appropriate force "extended" at 12V, it will also provide enough holding-force at 6V once it is retracted. Chances that the magnetic distance has halved between those situations is probable....