Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum http://www.raspberrypi.org/forums/viewtopic.php?p=583236#p583236
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 691 subscribers
  • Views 657 views
  • Users 0 members are here
  • raspberry_pi
Related

http://www.raspberrypi.org/forums/viewtopic.php?p=583236#p583236

grahamedriver
grahamedriver over 11 years ago

Hi

 

Would anyone like to comment on this circuit?

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 11 years ago

    I'm not too familiar with "current transfomers" I bought one a few years ago to experiment with, but haven't been able to find the time to do that yet.

     

    What I understand is that you need to provide a current path on the secondary side or otherwise the voltage on the current transformer will become very high.

     

    As the primary function of the current transformer is to transform the current, it will adapt the voltage to make that happen. If the diode is conducting: no problem. 0.6V extra on the secondary side. maybe about 0.6mV extra on the primary side.

     

    But when the diode blocks. no current can flow on the secondary side. So the voltage goes up until the diode starts conducting regardless of its efforts to try to block.... Not good. Provide an extra diode for that path. It would be pointing upwards and would be connected directly across the pins of the current transformer. Moving the zener to the other side of the diode would probably also work. You'd restrict the range by 0.6V, so if you can find a slightly larger-value zener, that'd be nice. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rew
    0 rew over 11 years ago

    I'm not too familiar with "current transfomers" I bought one a few years ago to experiment with, but haven't been able to find the time to do that yet.

     

    What I understand is that you need to provide a current path on the secondary side or otherwise the voltage on the current transformer will become very high.

     

    As the primary function of the current transformer is to transform the current, it will adapt the voltage to make that happen. If the diode is conducting: no problem. 0.6V extra on the secondary side. maybe about 0.6mV extra on the primary side.

     

    But when the diode blocks. no current can flow on the secondary side. So the voltage goes up until the diode starts conducting regardless of its efforts to try to block.... Not good. Provide an extra diode for that path. It would be pointing upwards and would be connected directly across the pins of the current transformer. Moving the zener to the other side of the diode would probably also work. You'd restrict the range by 0.6V, so if you can find a slightly larger-value zener, that'd be nice. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • grahamedriver
    0 grahamedriver over 11 years ago in reply to rew

    Hi

     

    I pretty much agree.

     

    Actually though I don't think the 0V6 reflects back into the primary, the current is what matters and that is not affected by the diode voltage

     

    In reverse bias? As you say not good.  Does the diode go open or short? If short the Zener is forward biased If open then what?  This is apparently a commercial product.  Did you look at the frequency range of the CT?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • grahamedriver
    0 grahamedriver over 11 years ago in reply to grahamedriver

    I hope I did not mark my own comment as "the correct answer"  I did not mean to do so.  And I don't seem to be able to mark any more a helpful - that's not helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 11 years ago in reply to grahamedriver

    graham driver wrote:

     

    Actually though I don't think the 0V6 reflects back into the primary, the current is what matters and that is not affected by the diode voltage

    It is a transformer. It transforms both current and voltage, but in opposite directions. So while a normal transformer is used in "voltage mode", you transform say 240V to 12V (say 20:1). When you load it with a current of say 1A, the primary current will be 1/20th of that.

     

    With a current transformer you do the opposite: you transform the current down. So if you have 1A primary, you get (with a 1000:1 current transformer) you'll get 1mA on the secondary side. In theory (with a perfect transformer): If you open circuit the secondary side, the transformer will work in voltage mode: zero current on the secondary side, so zero current on the primary side. So with zero current through the load, no voltage drop over the load, so, 220V over the transformer. i.e. an output voltage of 220V * 1000 = 220kV! This situation is to be avoided. :-)

     

    So for example you load the transformer with 1kOhm, so 1mA becomes 1V which is comfortably measurable. So now the output voltage is 1V, and therefore the input voltage must be 1:1000th, or 1mV. So this is the so-called burden that the current-measurement causes. Adding a 0.6V diode in series with the 1k resistor on the secondary side will add 0.6mV to the burden. Completely irrelevant compared to the 220V for the load, but still it's there.

     

    When the transformer is NOT perfect the resistance of the wire in the primary will probably cause a bigger voltage drop than the calculated burden from the theoretical transformer.....

     

    shabaz If you click on that picture you get a version that's plenty large. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to rew

    Roger Wolff wrote:


    If you click on that picture you get a version that's plenty large. :-)

     

    Ah, maybe that's only if you're a member, not sure..

    I registered on the day I saw a blog post that showed dangerous mains wiring, to suggest that perhaps the link should be removed or at least put up a warning.

    My comment was not published, and membership was not granted : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • grahamedriver
    0 grahamedriver over 11 years ago in reply to rew

    Hi

     

    Yes, I think... you are quite right

     

    What I was thinking, and what lead me astray, was that the diode drop does not affect the current, the voltage simply rises to overcome it.  But yes a CT is a transformer and must obey the rules. If there is more voltage in the secondary, more heat is being generated, the VI product has risen, and  that energy must come from somewhere -  there must be more energy extracted from the primary - more VI product -  more burden in the primary.

     

    Thank you for correcting my false thinking.

     

    I like the idea of moving the Zener, a diode pointing down as you say.  I was thinking of a bridge which might, or might not, be better but certainly costs more.  I will LTspice it.  I guess I will use a 1:500 transformer and ignore the frequency response of the 56100C for now -  www.murata-ps.com/data/magnetics/kmp_5600.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer