Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Does RPi B+ have high enough power output?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 709 subscribers
  • Views 2891 views
  • Users 0 members are here
  • b+
  • raspberry_pi
  • raspberrypi
Related

Does RPi B+ have high enough power output?

e14 Contributor
e14 Contributor over 11 years ago

I have just bought a RPi B+ and found it cannot power my WD My Passport 1TB USB3 drive. The drive just clicks rather than spins up.

 

I'm hoping that it is something I ma doing wrong. Do all the USB ports on the B+ provide the same power?

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 11 years ago

    There are a few considerations.

    The harddrive takes about 1A, or about 1.5 times more than the raspberry pi itself. So your powersupply must be able to provide 1.7A total. If you have a "2A" chinese powersupply, chances are it is powerful enough for a raspberry pi, but not for the pi plus the WD.

     

    Secondly, if you power the pi the normal way, there is a polyfuse that is supposed to prevent fires in case of overcurrent. This should limit the current of the 'pi plus --whatever it has on the USB ports-- to about 1A, or maybe 1.4A.

     

    The trick to using external (usb-powered) harddrives with the 'pi is to connect them to the pi through a powered hub.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to rew

    Roger,

     

    Thanks for the swift response. Are you talking about the B or the B+? Everything I've read about the B+ indicates that it should be able to power a disk. I do have a new 2A supply, so presumed it would all work.

     

    Sadly, not at the moment - even though, as you say, it does work through a power hub.

     

    Charles

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 11 years ago in reply to e14 Contributor

    Just out of curiosity, do you have the double usb plug? Or a single? USB (technically) is only supposed to supply 500 ma, much of time on the powered usb hubs they don't limit the current to the individual ports, so you can get the full current at any of the ports. They are non-compliant, but it is very common.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mconners
    0 mconners over 11 years ago in reply to e14 Contributor

    Just out of curiosity, do you have the double usb plug? Or a single? USB (technically) is only supposed to supply 500 ma, much of time on the powered usb hubs they don't limit the current to the individual ports, so you can get the full current at any of the ports. They are non-compliant, but it is very common.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mconners

    Mike,

     

    I'm using a double USB cable. Looks like USB2 (ie it's not blue).

     

    Charles