I have just bought a RPi B+ and found it cannot power my WD My Passport 1TB USB3 drive. The drive just clicks rather than spins up.
I'm hoping that it is something I ma doing wrong. Do all the USB ports on the B+ provide the same power?
I have just bought a RPi B+ and found it cannot power my WD My Passport 1TB USB3 drive. The drive just clicks rather than spins up.
I'm hoping that it is something I ma doing wrong. Do all the USB ports on the B+ provide the same power?
You will need to configure the Raspberry Pi B+ to output up to 1.2A via the USB ports. It is limited to 0.6A by default.
From: https://projects.drogon.net/testing-setting-the-usb-current-limiter-on-the-raspberry-pi-b/
"Additionally, it can also limit the total current drawn by the USB peripherals. This is 600mA by default, but can be increased to 1.2A via software.
...
The first way is via a new option in /boot/config.txt. Currently you can add:
safe_mode_gpio=4but note that this will become:
max_usb_current=1in subsequent updates. To do that requires a reboot of your Pi, however there is a 2nd way and that’s in software – because the actual switch is controlled via the Pi’s GPIO, we can do it from the command-line after the Pi has booted:
BCM_GPIO pin number 38 is the magic control pin.
Using the wiringPi gpio command, you can do the following:
gpio -g write 38 0 gpio -g mode 38 out
Good find. That is useful information.
Mike
Good find. That is useful information.
Mike