Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Does RPi B+ have high enough power output?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 709 subscribers
  • Views 2941 views
  • Users 0 members are here
  • b+
  • raspberry_pi
  • raspberrypi
Related

Does RPi B+ have high enough power output?

e14 Contributor
e14 Contributor over 11 years ago

I have just bought a RPi B+ and found it cannot power my WD My Passport 1TB USB3 drive. The drive just clicks rather than spins up.

 

I'm hoping that it is something I ma doing wrong. Do all the USB ports on the B+ provide the same power?

  • Sign in to reply
  • Cancel
  • wallarug
    0 wallarug over 11 years ago in reply to e14 Contributor

    BTW how big is the drive you are trying to get to work?  Maybe a 3.5" drive might not be able to get the required power (sometimes over 1.5A). 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You will need to configure the Raspberry Pi B+ to output up to 1.2A via the USB ports. It is limited to 0.6A by default.

     

    From: https://projects.drogon.net/testing-setting-the-usb-current-limiter-on-the-raspberry-pi-b/

     

    "Additionally, it can also limit the total current drawn by the USB peripherals. This is 600mA by default, but can be increased to 1.2A via software.

    ...

     

    The first way is via a new option in /boot/config.txt. Currently you can add:

    safe_mode_gpio=4

    but note that this will become:

    max_usb_current=1

    in subsequent updates. To do that requires a reboot of your Pi, however there is a 2nd way and that’s in software – because the actual switch is controlled via the Pi’s GPIO, we can do it from the command-line after the Pi has booted:

    BCM_GPIO pin number 38 is the magic control pin.

    Using the wiringPi gpio command, you can do the following:

    gpio -g write 38 0 gpio -g mode 38 out
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • rew
    0 rew over 11 years ago in reply to e14 Contributor

    Woops. Seems I haven't been paying attenion. That would certainly explain things....

     

    wallarug : https://www.google.nl/search?q=wd+passport&client=ubuntu-browser&es_sm=91&source=lnms&tbm=isch&sa=X&ei=b9H9U5LoJcSm0AXt8…

     

    The passport is a 2.5" drive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 11 years ago in reply to e14 Contributor

    Good find. That is useful information.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Shaun,

     

    Your response answered my question. I have got my usb disk working on a RPi B+ using a 2A supply with the usb disk plugged in directly into the RPi using a dual usb cable. I have a WiFi dongle in the third socket.

     

    I now have a great NAS device with LUKS encrypting the usb drive. I plan to put it in a friends house (with unlimited broadband) to back up my own data using rsync.

     

    Cool.

     

    Thanks

     

    Charles

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<