Raspberry Pi Forum Raspberry Pi web server using PiFace, getting "Bad file descriptor"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 684 subscribers
  • Views 798 views
  • Users 0 members are here
  • badfiledescriptor
  • raspberry-pi
  • cgi
Related

Raspberry Pi web server using PiFace, getting "Bad file descriptor"

Former Member
Former Member over 11 years ago

Hi

 

Using a Raspberry Pi Model B with PiFace. I have downloaded, built and installed the PiFace libraries and enabled the spi devices. I wrote a C program and can turn the relays on and off. That program also sends HTML to the stdout. Indeed when executed I see the HTML on stdout.

 

I have downloaded and installed Apache2. A simple 'Hello World' app runs when I hit the cgi-bin directory with a web-browser. When, I try to hit my c-program using the cgi-bin in my web browser, I get the HTML presented to my browser. I print the time to the webpage so that I know it is working. However, the PiFace IO does not work. If I just run the c-program from the CLI in the cgi-bin directory, it generates the HTML with the time-stamp and actually executes the IO operations.

 

I browse to the Apache2 error log and see this error message "ERROR: Can not send SPI messageBad file descriptor".

 

My c-program has execute permissions.

The spi_bcm2708 module is loaded as confirmed by lsmod.

I get crw-rw---T on both /dev/spidev0.0 and /dev/spidev0.1 when using ls -l /dev/spidev*

 

Any ideas for what else I need to do to make the IO operate under CGI?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • mconners
    0 mconners over 11 years ago

    Yeah, the problem is probably the apache (I'm guessing it is nobody) user doesn't have access to the SPI dev. I notice you said that the SPI dev has crw-rw--t, that means it has owner and group permission for read and write.

     

    Do an ls -al on /dev/spidev* and see what the group ownership is.

     

    You may need to add "nobody" to that group.

     

    BTW, the ls -al may produce something like

     

    crw-rw---- 1 root root 89, 0 Jan  1  1970 /dev/spidev0.0, which means root is the owner and root is the group (the second root indicates the group) You can change this on bootup, or add "nobody" to the "root" group.

     

    Google "adding a user to a group", but be careful, there are security implications, if this is just a "toy" program, or something local, no big deal, but if this is publicly accessible, be careful.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mconners
    0 mconners over 11 years ago

    Yeah, the problem is probably the apache (I'm guessing it is nobody) user doesn't have access to the SPI dev. I notice you said that the SPI dev has crw-rw--t, that means it has owner and group permission for read and write.

     

    Do an ls -al on /dev/spidev* and see what the group ownership is.

     

    You may need to add "nobody" to that group.

     

    BTW, the ls -al may produce something like

     

    crw-rw---- 1 root root 89, 0 Jan  1  1970 /dev/spidev0.0, which means root is the owner and root is the group (the second root indicates the group) You can change this on bootup, or add "nobody" to the "root" group.

     

    Google "adding a user to a group", but be careful, there are security implications, if this is just a "toy" program, or something local, no big deal, but if this is publicly accessible, be careful.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mconners
    0 mconners over 11 years ago in reply to mconners

    Also, the httpd.conf should give you the username that apache it running as, or you can do

     

    ps auxww | grep apache

     

    to see who the owner is, in /etc/apache2/envvars, I have

     

    export APACHE_RUN_USER=www-data

    export APACHE_RUN_GROUP=www-data

     

    defined on one of my machines, so you may want to edit that file.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to mconners

    Thank you Mike,

     

    www-data was the apache user. Changing the owner on the spi devices and the toggle application, now allows me to run toggle from my browser.