Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum connecting to internet on Raspberry Pi B+
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 705 subscribers
  • Views 732 views
  • Users 0 members are here
  • frontpage
  • raspberry_pi
  • raspberry-pi
Related

connecting to internet on Raspberry Pi B+

e14 Contributor
e14 Contributor over 11 years ago

I have just unboxed my first set of a raspberry pi b+ and dont know how connect it to the internet with my Ethernet connected through my main PC. Can you do this, and if so why is the internet not working if both are plugged in ( Cord ).

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 11 years ago

    Hi Brett,

     

    That's a little complicated, not majorly but certainly not plug-and play if you do that method (effectively involves setting up a small network and configuring up a DHCP server or static addressing) and is not the normal way to use it.

     

    Ordinarily you would use one of two options:

     

    1. Plug the Raspberry Pi (RPI) directly into one of the ports (known as switch ports) on your home router

    or

    2. Plug a Wi-Pi 802.11 (Wi-Fi) USB adapter into the RPI, and use this to connect to your home wireless network.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    I have a 802.11n usb wireless WiFi connector that came with my package... I don't know if I plug it in and maybe I have to install the drivers on my main PC or if I can just connect through WiFi config on the graphical interfaces' WiFi Config..

     

    Thanks again,

    Brett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Hi Brett,

     

    The drivers from your PC won't with with the RPI, because the RPI doesn't run x86 code, and the RPI doesn't run Windows (so the drivers would be incompatible).

    If you have a Wi-Pi, or if you bought from a supplier who took care with the selecting an appropriate product for the bundle, then you may be able to just plug in the device and not have to install any drivers.

    You can then configure from the graphical interface or from the command line.

    With the Wi-Pi, there is no need to install any drivers, they are already installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    After you plug in WiFi on your Raspberry Pi, enter a LSUSB in Terminal to see if it registers. Send back the part for the WiFi which will show chip set on WiFi...

    BTW, ethernet cannot plug from Raspberry Pi to PC!

     

     

    Clem

    http://www.element14.com/community/update-advanced-comment.jspa?id=132621