Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum White noise only output
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 674 subscribers
  • Views 569 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

White noise only output

Former Member
Former Member over 11 years ago

Hello, I've been working with the folks at the Volumio forum and I think my situation has them stumped as well.

 

I've got a RPi model B vers 2 and I installed the Wolfson Audio card onto it.

 

I flashed a version of Volumio that some of the folks over there had modified to include the wolfson drivers and that had worked for many of them.

 

Unfortunately after many tries and several different versions of the Volumio image the best I can get is white noise through the line out or headphone out.

 

Here is the output from the dmesg command - I hope someone can help me.


Volumio 1.4 wolfson image - edited config.txt to kernel=kernel_new.img - changed the mixer setting to software and ran dmesg.


Here is the output:


[    0.000000] Booting Linux on physical CPU 0x0

[    0.000000] Initializing cgroup subsys cpu

[    0.000000] Initializing cgroup subsys cpuacct

[    0.000000] Linux version 3.12.13-rt21+ (georg@musicbox) (gcc version 4.8.3 20140106 (prerelease) (crosstool-NG linaro-1.13.1-4.8-2014.01 - Linaro GCC 2013.11) ) #1 PREEMPT RT Thu Mar 27 16:58:09 CET 2014

[    0.000000] CPU: ARMv6-compatible processor [410fb767] revision 7 (ARMv7), cr=00c5387d

[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT nonaliasing instruction cache

[    0.000000] Machine: BCM2708

[    0.000000] Memory policy: ECC disabled, Data cache writeback

[    0.000000] On node 0 totalpages: 126976

[    0.000000] free_area_init_node: node 0, pgdat c069a0e4, node_mem_map c074e000

[    0.000000]   Normal zone: 992 pages used for memmap

[    0.000000]   Normal zone: 0 pages reserved

[    0.000000]   Normal zone: 126976 pages, LIFO batch:31

[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768

[    0.000000] pcpu-alloc: [0] 0

[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125984

[    0.000000] Kernel command line: dma.dmachans=0x7f35 bcm2708_fb.fbwidth=1184 bcm2708_fb.fbheight=624 bcm2708.boardrev=0xe bcm2708.serial=0xd2fba881 smsc95xx.macaddr=B8:27:EB:FB:A8:81 sdhci-bcm2708.emmc_clock_freq=250000000 vc_mem.mem_base=0x1fa00000 vc_mem.mem_size=0x20000000  force_turbo=1 dwc_otg.lpm_enable=0 console=ttyAMA0,115200 kgdboc=ttyAMA0,115200 console=tty1 root=/dev/mmcblk0p3 elevator=noop rootfstype=ext4 rootwait smsc95xx.turbo_mode=N

[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)

[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

[    0.000000] allocated 3555328 bytes of page_cgroup

[    0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups

[    0.000000] Memory: 492520K/507904K available (4500K kernel code, 299K rwdata, 1780K rodata, 147K init, 714K bss, 15384K reserved)

[    0.000000] Virtual kernel memory layout:

[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

[    0.000000]     vmalloc : 0xdf800000 - 0xff000000   ( 504 MB)

[    0.000000]     lowmem  : 0xc0000000 - 0xdf000000   ( 496 MB)

[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)

[    0.000000]       .text : 0xc0008000 - 0xc062a294   (6281 kB)

[    0.000000]       .init : 0xc062b000 - 0xc064fe54   ( 148 kB)

[    0.000000]       .data : 0xc0650000 - 0xc069acc8   ( 300 kB)

[    0.000000]        .bss : 0xc069acd4 - 0xc074d648   ( 715 kB)

[    0.000000] SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

[    0.000000] Preemptible hierarchical RCU implementation.

[    0.000000] NR_IRQS:460

[    0.000000] sched_clock: 32 bits at 1000kHz, resolution 1000ns, wraps every 4294967ms

[    0.000000] Switching to timer-based delay loop

[    0.000000] Console: colour dummy device 80x30

[    0.000000] console [tty1] enabled

[    0.001388] Calibrating delay loop (skipped), value calculated using timer frequency.. 2.00 BogoMIPS (lpj=10000)

[    0.001393] pid_max: default: 32768 minimum: 301

[    0.001936] Mount-cache hash table entries: 512

[    0.002774] Initializing cgroup subsys memory

[    0.002856] Initializing cgroup subsys devices

[    0.002865] Initializing cgroup subsys freezer

[    0.002873] Initializing cgroup subsys blkio

[    0.003017] CPU: Testing write buffer coherency: ok

[    0.003420] Setting up static identity map for 0xc04475c0 - 0xc044761c

[    0.006245] devtmpfs: initialized

[    0.018956] VFP support v0.3: implementor 41 architecture 1 part 20 variant b rev 5

[    0.019873] regulator-dummy: no parameters

[    0.020494] NET: Registered protocol family 16

[    0.025496] DMA: preallocated 4096 KiB pool for atomic coherent allocations

[    0.026171] cpuidle: using governor ladder

[    0.026220] cpuidle: using governor menu

[    0.026703] bcm2708.uart_clock = 0

[    0.028875] hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

[    0.028934] hw-breakpoint: maximum watchpoint size is 4 bytes.

[    0.028971] mailbox: Broadcom VideoCore Mailbox driver

[    0.029350] bcm2708_vcio: mailbox at f200b880

[    0.029496] bcm_power: Broadcom power driver

[    0.029536] bcm_power_open() -> 0

[    0.029562] bcm_power_request(0, 8)

[    0.530294] bcm_mailbox_read -> 00000080, 0

[    0.530340] bcm_power_request -> 0

[    0.530634] Serial: AMBA PL011 UART driver

[    0.530801] dev:f1: ttyAMA0 at MMIO 0x20201000 (irq = 83, base_baud = 0) is a PL011 rev3

[    0.906639] console [ttyAMA0] enabled

[    0.936711] bio: create slab <bio-0> at 0

[    0.942059] platform bcm2708-dmaengine: Driver bcm2708-dmaengine requests probe deferral

[    0.950433] DC_3V3: 1800 mV

[    0.953629] DC_5V: 5000 mV

[    0.957101] SCSI subsystem initialized

[    0.961090] usbcore: registered new interface driver usbfs

[    0.966701] usbcore: registered new interface driver hub

[    0.972303] usbcore: registered new device driver usb

[    0.977902] Advanced Linux Sound Architecture Driver Initialized.

[    0.985240] Switched to clocksource stc

[    0.989567] FS-Cache: Loaded

[    0.992772] CacheFiles: Loaded

[    1.010140] NET: Registered protocol family 2

[    1.015837] TCP established hash table entries: 4096 (order: 3, 32768 bytes)

[    1.023064] TCP bind hash table entries: 4096 (order: 4, 98304 bytes)

[    1.029765] TCP: Hash tables configured (established 4096 bind 4096)

[    1.036228] TCP: reno registered

[    1.039490] UDP hash table entries: 256 (order: 2, 16384 bytes)

[    1.045481] UDP-Lite hash table entries: 256 (order: 2, 16384 bytes)

[    1.052418] NET: Registered protocol family 1

[    1.057486] RPC: Registered named UNIX socket transport module.

[    1.063448] RPC: Registered udp transport module.

[    1.068169] RPC: Registered tcp transport module.

[    1.072891] RPC: Registered tcp NFSv4.1 backchannel transport module.

[    1.080356] bcm2708_dma: DMA manager at f2007000

[    1.085115] bcm2708_gpio: bcm2708_gpio_probe c065e080

[    1.090680] vc-mem: phys_addr:0x00000000 mem_base=0x1fa00000 mem_size:0x20000000(512 MiB)

[    1.100263] audit: initializing netlink socket (disabled)

[    1.105771] type=2000 audit(1.100:1): initialized

[    1.292030] VFS: Disk quotas dquot_6.5.2

[    1.296338] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

[    1.306038] FS-Cache: Netfs 'nfs' registered for caching

[    1.312919] NFS: Registering the id_resolver key type

[    1.318093] Key type id_resolver registered

[    1.322299] Key type id_legacy registered

[    1.327107] msgmni has been set to 961

[    1.333313] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)

[    1.341144] io scheduler noop registered (default)

[    1.345980] io scheduler deadline registered

[    1.350631] io scheduler cfq registered

[    1.354882] bcm2708_fb_debugfs_init: could not create debugfs entry

[    1.361287] BCM2708FB: allocated DMA memory 5e9a0000

[    1.366543] BCM2708FB: allocated DMA channel 0 @ f2007000

[    1.380837] Console: switching to colour frame buffer device 148x39

[    1.393290] uart-pl011 dev:f1: no DMA platform data

[    1.398315] kgdb: Registered I/O driver kgdboc.

[    1.403635] vc-cma: Videocore CMA driver

[    1.407660] vc-cma: vc_cma_base      = 0x00000000

[    1.414731] vc-cma: vc_cma_size      = 0x00000000 (0 MiB)

[    1.422609] vc-cma: vc_cma_initial   = 0x00000000 (0 MiB)

[    1.441596] brd: module loaded

[    1.453258] loop: module loaded

[    1.459176] vchiq: vchiq_init_state: slot_zero = 0xdf804000, is_master = 0

[    1.469522] Loading iSCSI transport class v2.0-870.

[    1.478674] bcm2708_spi bcm2708_spi.0: master is unqueued, this is deprecated

[    1.491427] LDO1: 1200 <--> 1800 mV at 1800 mV

[    1.498413] LDO1: supplied by DC_3V3

[    1.526836] arizona spi0.1: WM5102 revision C

[    1.546679] MICVDD: 1700 <--> 3300 mV at 3000 mV

[    1.553844] MICVDD: supplied by DC_3V3

[    1.560332] gpiochip_find_base: cannot find free range

[    1.567782] gpiochip_add: gpios -1..3 (arizona) failed to register

[    1.576266] arizona-gpio arizona-gpio: Could not register gpiochip, -28

[    1.585185] arizona-gpio: probe of arizona-gpio failed with error -28

[    1.594754] bcm2708_spi bcm2708_spi.0: SPI Controller at 0x20204000 (irq 80)

[    1.604501] usbcore: registered new interface driver smsc95xx

[    1.612722] dwc_otg: version 3.00a 10-AUG-2012 (platform bus)

[    1.821019] Core Release: 2.80a

[    1.826555] Setting default values for core params

[    1.833692] Finished setting default values for core params

[    2.041949] Using Buffer DMA mode

[    2.047559] Periodic Transfer Interrupt Enhancement - disabled

[    2.055733] Multiprocessor Interrupt Enhancement - disabled

[    2.063622] OTG VER PARAM: 0, OTG VER FLAG: 0

[    2.070388] Dedicated Tx FIFOs mode

[    2.076611] dwc_otg: Microframe scheduler enabled

[    2.076671] dwc_otg bcm2708_usb: DWC OTG Controller

[    2.083988] dwc_otg bcm2708_usb: new USB bus registered, assigned bus number 1

[    2.093981] dwc_otg bcm2708_usb: irq 32, io mem 0x00000000

[    2.101973] Init: Port Power? op_state=1

[    2.108210] Init: Power Port (0)

[    2.113967] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

[    2.123261] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

[    2.132914] usb usb1: Product: DWC OTG Controller

[    2.140126] usb usb1: Manufacturer: Linux 3.12.13-rt21+ dwc_otg_hcd

[    2.148776] usb usb1: SerialNumber: bcm2708_usb

[    2.156714] hub 1-0:1.0: USB hub found

[    2.162966] hub 1-0:1.0: 1 port detected

[    2.170080] dwc_otg: FIQ enabled

[    2.170102] dwc_otg: NAK holdoff enabled

[    2.170111] dwc_otg: FIQ split fix enabled

[    2.170132] Module dwc_common_port init

[    2.170642] usbcore: registered new interface driver usb-storage

[    2.179520] mousedev: PS/2 mouse device common for all mice

[    2.187517] i2c /dev entries driver

[    2.193544] bcm2708_i2c_init_pinmode(0,0)

[    2.200109] bcm2708_i2c_init_pinmode(0,1)

[    2.207133] bcm2708_i2c bcm2708_i2c.0: BSC0 Controller at 0x20205000 (irq 79) (baudrate 100k)

[    2.218151] bcm2708_i2c_init_pinmode(1,2)

[    2.224577] bcm2708_i2c_init_pinmode(1,3)

[    2.231814] bcm2708_i2c bcm2708_i2c.1: BSC1 Controller at 0x20804000 (irq 79) (baudrate 100k)

[    2.243718] bcm2835-cpufreq: min=700000 max=700000 cur=700000

[    2.252116] bcm2835-cpufreq: switching to governor powersave

[    2.260155] bcm2835-cpufreq: switching to governor powersave

[    2.268254] sdhci: Secure Digital Host Controller Interface driver

[    2.276785] sdhci: Copyright(c) Pierre Ossman

[    2.283568] sdhci: Enable low-latency mode

[    2.290420] mmc0: no vqmmc regulator found

[    2.296783] mmc0: no vmmc regulator found

[    2.345413] mmc0: SDHCI controller on BCM2708_Arasan [platform] using platform's DMA

[    2.365083] mmc0: BCM2708 SDHC host at 0x20300000 DMA 2 IRQ 77

[    2.365521] Indeed it is in host mode hprt0 = 00021501

[    2.413028] sdhci-pltfm: SDHCI platform and OF driver helper

[    2.432856] hidraw: raw HID events driver (C) Jiri Kosina

[    2.437454] mmc0: new high speed SDHC card at address aaaa

[    2.445385] mmcblk0: mmc0:aaaa SL16G 14.8 GiB

[    2.446940]  mmcblk0: p1 p3

[    2.486829] usbcore: registered new interface driver usbhid

[    2.494765] usbhid: USB HID core driver

[    2.501179] platform arizona-extcon: Driver arizona-extcon requests probe deferral

[    2.512557] ------------[ cut here ]------------

[    2.519653] WARNING: CPU: 0 PID: 1 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()

[    2.529639] sysfs: cannot create duplicate filename '/devices/platform/bcm2708_spi.0/spi_master/spi0/spi0.1/regulator/regulator.3/spi0.1-DCVDD'

[    2.545064] Modules linked in:

[    2.550729] CPU: 0 PID: 1 Comm: swapper Not tainted 3.12.13-rt21+ #1

[    2.559744] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)

[    2.570978] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)

[    2.582658] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)

[    2.595086] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)

[    2.605385] usb 1-1: new high-speed USB device number 2 using dwc_otg

[    2.605680] Indeed it is in host mode hprt0 = 00001101

[    2.642891] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)

[    2.675337] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)

[    2.696804] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)

[    2.717585] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)

[    2.729842] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0373064>] (wm_adsp2_init+0x5c/0x13c)

[    2.743749] [<c0373064>] (wm_adsp2_init+0x5c/0x13c) from [<c0370d78>] (wm5102_probe+0x90/0x188)

[    2.757516] [<c0370d78>] (wm5102_probe+0x90/0x188) from [<c02854e0>] (really_probe+0x60/0x1e4)

[    2.770957] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0285750>] (__driver_attach+0x98/0x9c)

[    2.784696] [<c0285750>] (__driver_attach+0x98/0x9c) from [<c0283a84>] (bus_for_each_dev+0x60/0x94)

[    2.798987] [<c0283a84>] (bus_for_each_dev+0x60/0x94) from [<c0284d5c>] (bus_add_driver+0x1c4/0x274)

[    2.813206] [<c0284d5c>] (bus_add_driver+0x1c4/0x274) from [<c0285d54>] (driver_register+0x78/0xf8)

[    2.827508] [<c0285d54>] (driver_register+0x78/0xf8) from [<c000861c>] (do_one_initcall+0x114/0x178)

[    2.841784] [<c000861c>] (do_one_initcall+0x114/0x178) from [<c062bb74>] (kernel_init_freeable+0xf4/0x1b4)

[    2.857120] [<c062bb74>] (kernel_init_freeable+0xf4/0x1b4) from [<c043c51c>] (kernel_init+0x8/0x150)

[    2.866256] usb 1-1: New USB device found, idVendor=0424, idProduct=9512

[    2.866327] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0

[    2.895685] [<c043c51c>] (kernel_init+0x8/0x150) from [<c000e058>] (ret_from_fork+0x14/0x3c)

[    2.909440] ---[ end trace 0000000000000001 ]---

[    2.920377] LDO1: could not add device link spi0.1 err -17

[    2.921083] hub 1-1:1.0: USB hub found

[    2.921374] hub 1-1:1.0: 3 ports detected

[    2.952773] LDO1: Failed to create debugfs directory

[    2.970969] bcm2708-i2s bcm2708-i2s.0: Failed to create debugfs directory

[    3.195514] usb 1-1.1: new high-speed USB device number 3 using dwc_otg

[    3.316200] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00

[    3.335305] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0

[    3.358329] smsc95xx v1.0.4

[    3.434174] smsc95xx 1-1.1:1.0 eth0: register 'smsc95xx' at usb-bcm2708_usb-1.1, smsc95xx USB 2.0 Ethernet, b8:27:eb:fb:a8:81

[    3.545565] usb 1-1.2: new full-speed USB device number 4 using dwc_otg

[    3.677600] usb 1-1.2: New USB device found, idVendor=046d, idProduct=c52b

[    3.696434] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0

[    3.715561] usb 1-1.2: Product: USB Receiver

[    3.722973] usb 1-1.2: Manufacturer: Logitech

[    3.767474] input: Logitech USB Receiver as /devices/platform/bcm2708_usb/usb1/1-1/1-1.2/1-1.2:1.0/input/input0

[    3.790274] hid-generic 0003:046D:C52B.0001: input,hidraw0: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-bcm2708_usb-1.2/input0

[    3.846437] input: Logitech USB Receiver as /devices/platform/bcm2708_usb/usb1/1-1/1-1.2/1-1.2:1.1/input/input1

[    3.867764] hid-generic 0003:046D:C52B.0002: input,hiddev0,hidraw1: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-bcm2708_usb-1.2/input1

[    3.912972] hid-generic 0003:046D:C52B.0003: hiddev0,hidraw2: USB HID v1.11 Device [Logitech USB Receiver] on usb-bcm2708_usb-1.2/input2

[    4.025603] usb 1-1.3: new high-speed USB device number 5 using dwc_otg

[    4.137164] usb 1-1.3: New USB device found, idVendor=1e3d, idProduct=2096

[    4.149013] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3

[    4.165363] usb 1-1.3: Product: Flash Disk     

[    4.177145] usb 1-1.3: Manufacturer: Generic

[    4.190295] usb 1-1.3: SerialNumber: CCBB1108020140313241603106

[    4.206480] usb-storage 1-1.3:1.0: USB Mass Storage device detected

[    4.223932] scsi0 : usb-storage 1-1.3:1.0

[    5.004296] wm8804 1-003a: revision E

[    5.013429] bcm2708-i2s bcm2708-i2s.0: ASoC: pcm constructor failed: -517

[    5.024049] snd-rpi-wsp snd-rpi-wsp.0: ASoC: can't create pcm WM5102 AiFi :-517

[    5.034711] snd-rpi-wsp snd-rpi-wsp.0: ASoC: failed to instantiate card -517

[    5.057394] snd-rpi-wsp snd-rpi-wsp.0: Failed to register card: -517

[    5.067236] platform snd-rpi-wsp.0: Driver snd-rpi-wsp requests probe deferral

[    5.079079] TCP: cubic registered

[    5.085794] Initializing XFRM netlink socket

[    5.093740] NET: Registered protocol family 17

[    5.102298] Key type dns_resolver registered

[    5.111669] registered taskstats version 1

[    5.121239] platform arizona-extcon: Driver arizona-extcon requests probe deferral

[    5.226857] scsi 0:0:0:0: Direct-Access     Generic  Flash Disk       5.00 PQ: 0 ANSI: 2

[    5.247102] sd 0:0:0:0: [sda] 3913728 512-byte logical blocks: (2.00 GB/1.86 GiB)

[    5.263106] sd 0:0:0:0: [sda] Write Protect is off

[    5.272988] sd 0:0:0:0: [sda] Mode Sense: 0b 00 00 08

[    5.274037] sd 0:0:0:0: [sda] No Caching mode page found

[    5.286464] sd 0:0:0:0: [sda] Assuming drive cache: write through

[    5.306960] sd 0:0:0:0: [sda] No Caching mode page found

[    5.318299] sd 0:0:0:0: [sda] Assuming drive cache: write through

[    5.330221]  sda: sda1

[    5.346245] sd 0:0:0:0: [sda] No Caching mode page found

[    5.358043] sd 0:0:0:0: [sda] Assuming drive cache: write through

[    5.370051] sd 0:0:0:0: [sda] Attached SCSI removable disk

[    6.199061] ------------[ cut here ]------------

[    6.206576] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()

[    6.216963] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.0/regulator/regulator.1/wm5102-codec-DBVDD2'

[    6.231772] Modules linked in:

[    6.237755] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G        W    3.12.13-rt21+ #1

[    6.248672] Workqueue: deferwq deferred_probe_work_func

[    6.257259] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)

[    6.268751] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)

[    6.280954] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)

[    6.293589] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)

[    6.306103] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)

[    6.318899] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)

[    6.332121] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)

[    6.344875] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)

[    6.357482] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)

[    6.371238] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)

[    6.385599] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)

[    6.399061] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)

[    6.412507] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)

[    6.426476] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)

[    6.439132] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)

[    6.451578] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)

[    6.464428] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)

[    6.476967] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)

[    6.490680] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)

[    6.504144] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)

[    6.517080] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)

[    6.529379] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)

[    6.541274] ---[ end trace 0000000000000003 ]---

[    6.549833] DC_3V3: could not add device link wm5102-codec err -17

[    6.560036] DC_3V3: Failed to create debugfs directory

[    6.569037] ------------[ cut here ]------------

[    6.577494] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()

[    6.588922] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.0/regulator/regulator.1/wm5102-codec-DBVDD3'

[    6.605022] Modules linked in:

[    6.611958] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G        W    3.12.13-rt21+ #1

[    6.623981] Workqueue: deferwq deferred_probe_work_func

[    6.633345] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)

[    6.645914] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)

[    6.659046] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)

[    6.672760] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)

[    6.685672] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)

[    6.699432] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)

[    6.713681] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)

[    6.726896] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)

[    6.740162] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)

[    6.754516] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)

[    6.769544] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)

[    6.783520] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)

[    6.797534] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)

[    6.811851] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)

[    6.825333] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)

[    6.838112] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)

[    6.851051] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)

[    6.864060] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)

[    6.877954] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)

[    6.892039] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)

[    6.905489] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)

[    6.917633] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)

[    6.929819] ---[ end trace 0000000000000004 ]---

[    6.938289] DC_3V3: could not add device link wm5102-codec err -17

[    6.948249] DC_3V3: Failed to create debugfs directory

[    6.957474] ------------[ cut here ]------------

[    6.966081] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()

[    6.977723] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.0/regulator/regulator.1/wm5102-codec-CPVDD'

[    6.993599] Modules linked in:

[    7.000895] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G        W    3.12.13-rt21+ #1

[    7.012555] Workqueue: deferwq deferred_probe_work_func

[    7.021774] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)

[    7.034452] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)

[    7.047544] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)

[    7.061088] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)

[    7.074302] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)

[    7.087794] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)

[    7.101631] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)

[    7.115044] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)

[    7.128547] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)

[    7.142705] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)

[    7.157694] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)

[    7.171828] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)

[    7.185951] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)

[    7.200045] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)

[    7.213147] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)

[    7.226422] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)

[    7.239216] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)

[    7.251926] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)

[    7.266016] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)

[    7.279918] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)

[    7.293008] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)

[    7.305537] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)

[    7.317449] ---[ end trace 0000000000000005 ]---

[    7.326134] DC_3V3: could not add device link wm5102-codec err -17

[    7.336386] DC_3V3: Failed to create debugfs directory

[    7.345377] ------------[ cut here ]------------

[    7.353841] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()

[    7.365348] sysfs: cannot create duplicate filename '/devices/platform/bcm2708_spi.0/spi_master/spi0/spi0.1/regulator/regulator.4/wm5102-codec-MICVDD'

[    7.386901] Modules linked in:

[    7.393953] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G        W    3.12.13-rt21+ #1

[    7.405691] Workqueue: deferwq deferred_probe_work_func

[    7.414935] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)

[    7.427549] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)

[    7.440651] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)

[    7.454079] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)

[    7.467339] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)

[    7.481219] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)

[    7.495111] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)

[    7.508291] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)

[    7.521702] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)

[    7.535879] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)

[    7.550651] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)

[    7.564779] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)

[    7.579041] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)

[    7.593319] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)

[    7.606501] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)

[    7.619361] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)

[    7.632371] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)

[    7.645253] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)

[    7.659333] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)

[    7.673381] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)

[    7.686498] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)

[    7.698833] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)

[    7.710942] ---[ end trace 0000000000000006 ]---

[    7.719463] MICVDD: could not add device link wm5102-codec err -17

[    7.729493] MICVDD: Failed to create debugfs directory

[    7.738604] ------------[ cut here ]------------

[    7.747009] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()

[    7.758676] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.1/regulator/regulator.2/wm5102-codec-SPKVDDL'

[    7.774865] Modules linked in:

[    7.781821] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G        W    3.12.13-rt21+ #1

[    7.793684] Workqueue: deferwq deferred_probe_work_func

[    7.802847] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)

[    7.815556] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)

[    7.828482] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)

[    7.842220] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)

[    7.855173] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)

[    7.868735] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)

[    7.882901] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)

[    7.896321] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)

[    7.909519] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)

[    7.923867] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)

[    7.938886] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)

[    7.952916] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)

[    7.966939] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)

[    7.981104] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)

[    7.994629] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)

[    8.007707] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)

[    8.020449] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)

[    8.033421] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)

[    8.047318] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)

[    8.061221] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)

[    8.074624] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)

[    8.086955] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)

[    8.098987] ---[ end trace 0000000000000007 ]---

[    8.107624] DC_5V: could not add device link wm5102-codec err -17

[    8.117738] DC_5V: Failed to create debugfs directory

[    8.126935] ------------[ cut here ]------------

[    8.135445] WARNING: CPU: 0 PID: 6 at fs/sysfs/dir.c:526 sysfs_add_one+0x88/0xb0()

[    8.146890] sysfs: cannot create duplicate filename '/devices/platform/reg-fixed-voltage.1/regulator/regulator.2/wm5102-codec-SPKVDDR'

[    8.163108] Modules linked in:

[    8.170439] CPU: 0 PID: 6 Comm: kworker/u2:0 Tainted: G        W    3.12.13-rt21+ #1

[    8.182003] Workqueue: deferwq deferred_probe_work_func

[    8.191288] [<c0014738>] (unwind_backtrace+0x0/0xec) from [<c001188c>] (show_stack+0x10/0x14)

[    8.203675] [<c001188c>] (show_stack+0x10/0x14) from [<c001f4bc>] (warn_slowpath_common+0x68/0x88)

[    8.216877] [<c001f4bc>] (warn_slowpath_common+0x68/0x88) from [<c001f50c>] (warn_slowpath_fmt+0x30/0x40)

[    8.230408] [<c001f50c>] (warn_slowpath_fmt+0x30/0x40) from [<c0138878>] (sysfs_add_one+0x88/0xb0)

[    8.243604] [<c0138878>] (sysfs_add_one+0x88/0xb0) from [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8)

[    8.257486] [<c01391d0>] (sysfs_do_create_link_sd+0xbc/0x1e8) from [<c02587ac>] (create_regulator+0xb4/0x288)

[    8.271327] [<c02587ac>] (create_regulator+0xb4/0x288) from [<c0258a20>] (_regulator_get+0xa0/0x164)

[    8.284383] [<c0258a20>] (_regulator_get+0xa0/0x164) from [<c0258b34>] (devm_regulator_get+0x38/0x6c)

[    8.297986] [<c0258b34>] (devm_regulator_get+0x38/0x6c) from [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278)

[    8.312161] [<c0365ad8>] (snd_soc_dapm_new_control+0x1d0/0x278) from [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84)

[    8.327060] [<c0365cf4>] (snd_soc_dapm_new_controls+0x44/0x84) from [<c036301c>] (soc_probe_codec+0x10c/0x300)

[    8.341129] [<c036301c>] (soc_probe_codec+0x10c/0x300) from [<c0364070>] (snd_soc_register_card+0xa44/0x14cc)

[    8.355270] [<c0364070>] (snd_soc_register_card+0xa44/0x14cc) from [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420)

[    8.369582] [<c037579c>] (snd_rpi_wsp_probe+0x2d0/0x420) from [<c02854e0>] (really_probe+0x60/0x1e4)

[    8.382719] [<c02854e0>] (really_probe+0x60/0x1e4) from [<c0283b24>] (bus_for_each_drv+0x58/0x8c)

[    8.395853] [<c0283b24>] (bus_for_each_drv+0x58/0x8c) from [<c0285474>] (device_attach+0x74/0x80)

[    8.408914] [<c0285474>] (device_attach+0x74/0x80) from [<c0284a68>] (bus_probe_device+0x84/0xac)

[    8.421618] [<c0284a68>] (bus_probe_device+0x84/0xac) from [<c0284f64>] (deferred_probe_work_func+0x60/0x8c)

[    8.435632] [<c0284f64>] (deferred_probe_work_func+0x60/0x8c) from [<c0033d4c>] (process_one_work+0xf8/0x344)

[    8.449755] [<c0033d4c>] (process_one_work+0xf8/0x344) from [<c0034740>] (worker_thread+0x12c/0x3ac)

[    8.462886] [<c0034740>] (worker_thread+0x12c/0x3ac) from [<c0039e70>] (kthread+0x9c/0xa4)

[    8.475341] [<c0039e70>] (kthread+0x9c/0xa4) from [<c000e058>] (ret_from_fork+0x14/0x3c)

[    8.487514] ---[ end trace 0000000000000008 ]---

[    8.495955] DC_5V: could not add device link wm5102-codec err -17

[    8.505941] DC_5V: Failed to create debugfs directory

[    8.516191] genirq: Flags mismatch irq 404. 00002000 (Thermal warning) vs. 00002000 (Thermal warning)

[    8.516235] arizona spi0.1: Failed to get thermal warning IRQ: -16

[    8.539859] genirq: Flags mismatch irq 405. 00002000 (Thermal shutdown) vs. 00002000 (Thermal shutdown)

[    8.539894] arizona spi0.1: Failed to get thermal shutdown IRQ: -16

[    9.357971] wm8804 1-003a: revision E

[    9.370678] snd-rpi-wsp snd-rpi-wsp.0:  wm5102-aif1 <-> bcm2708-i2s.0 mapping ok

[    9.635324] arizona spi0.1: FLL1: Timed out waiting for lock

[    9.751283] input: Headset as /devices/platform/bcm2708_spi.0/spi_master/spi0/spi0.1/arizona-extcon/input/input2

[    9.765733] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

[    9.779653] ALSA device list:

[    9.786824]   #0: snd_rpi_wsp

[    9.793489]   #1: bcm2835 ALSA

[    9.817235] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)

[    9.829353] VFS: Mounted root (ext4 filesystem) on device 179:3.

[    9.849958] devtmpfs: mounted

[    9.857334] Freeing unused kernel memory: 144K (c062b000 - c064f000)

[   11.706818] udevd[178]: starting version 175

[   17.279454] FAT-fs (sda1): utf8 is not a recommended IO charset for FAT filesystems, filesystem will be case sensitive!

[   22.426633] EXT4-fs (mmcblk0p3): re-mounted. Opts: (null)

[   22.984120] EXT4-fs (mmcblk0p3): Mount option "nouser_xattr" will be removed by 3.5

[   22.984120] Contact linux-ext4@vger.kernel.org if you think we should keep it.

[   22.984120]

[   23.013262] EXT4-fs (mmcblk0p3): re-mounted. Opts: nouser_xattr,errors=remount-ro

[   30.557712] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.

[   33.920234] NET: Registered protocol family 10

[   34.383429] smsc95xx 1-1.1:1.0 eth0: hardware isn't capable of remote wakeup

[   34.396243] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

[   36.005659] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

[   36.009996] smsc95xx 1-1.1:1.0 eth0: link up, 100Mbps, full-duplex, lpa 0xCDE1

[   44.751296] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).

[  206.942589] bcm2835-cpufreq: switching to governor performance

[  206.952880] bcm2835-cpufreq: switching to governor performance

[  208.515088] arizona spi0.1: FLL1: Timed out waiting for lock

[  208.532148] bcm2708-i2s bcm2708-i2s.0: I2S SYNC error!

[  310.227715] EXT4-fs (mmcblk0p3): error count: 3

[  310.236615] EXT4-fs (mmcblk0p3): initial error at 1396987247: mb_free_blocks:1426: block 309248

[  310.249886] EXT4-fs (mmcblk0p3): last error at 1396987322: ext4_remount:4680

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Problem solved - it was a bug in the volumio wolfson image that I used. Some internet radio stations won't play at all, some give white noise and others play just fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Hi

     

    I am facing the same problem with kernel 3.12.13-rt21+. So what was the solution for this bug? Did you switch to a different kernel or fixed this problem in 3.12.13-rt21+?

     

    Thank you in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Hi

     

    I am facing the same problem with kernel 3.12.13-rt21+. So what was the solution for this bug? Did you switch to a different kernel or fixed this problem in 3.12.13-rt21+?

     

    Thank you in advance