Raspberry Pi Forum What is the maximum class memory Pi can support.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 685 subscribers
  • Views 959 views
  • Users 0 members are here
  • memory
Related

What is the maximum class memory Pi can support.

Former Member
Former Member over 11 years ago

I have heard Class 4 is the max but I have also heard that for audio must be Class 10 or better.

I found a link and its a bit sketchy as I found discrepant rating on the same SanDisk product I am attempting to use 32 class10 also look slike not all OS's are equal here

RPi SD cards - eLinux.org

Is there an optimal "chip" that supports the most OS's and runs fast Is the Proper Question.

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 11 years ago

    Just after the introduction of the 'pi there was a problem with class 10 cards: Linux would ask: "do you support the new fancy fast transfer mode?" and the card would say (it has to if it is class 10) YES! and then Linux would say: "OK! Lets do that then!".... forgetting that the pi hardware cannot do this....

     

    This might be the origin of tales that say not to buy a class 10 card. As far as I know this has been fixed for 2.5 years now.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rew
    0 rew over 11 years ago

    Just after the introduction of the 'pi there was a problem with class 10 cards: Linux would ask: "do you support the new fancy fast transfer mode?" and the card would say (it has to if it is class 10) YES! and then Linux would say: "OK! Lets do that then!".... forgetting that the pi hardware cannot do this....

     

    This might be the origin of tales that say not to buy a class 10 card. As far as I know this has been fixed for 2.5 years now.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Problemchild
    0 Problemchild over 11 years ago in reply to rew

    I used them from Day 1 no problems at least with my SAN Disk ones .....

    But yes no one has really complained for ages.