Raspberry Pi Forum What is the maximum class memory Pi can support.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 685 subscribers
  • Views 959 views
  • Users 0 members are here
  • memory
Related

What is the maximum class memory Pi can support.

Former Member
Former Member over 11 years ago

I have heard Class 4 is the max but I have also heard that for audio must be Class 10 or better.

I found a link and its a bit sketchy as I found discrepant rating on the same SanDisk product I am attempting to use 32 class10 also look slike not all OS's are equal here

RPi SD cards - eLinux.org

Is there an optimal "chip" that supports the most OS's and runs fast Is the Proper Question.

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 11 years ago

    Yeah I used some 32GB class 10s from SanDisk and a few other brands ...Yes a few don't work but the speed is only a part of the problem.

    My advice is the same as many others buy one find it works ...stick with it.

     

    Also if you are having problems from the start  I would also make sure to use the writing program under windows which has a verify or have a Block Size (BS=128k) or similar using DD under Linux so that the writing speed is kept reasonable

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 11 years ago

    Yeah I used some 32GB class 10s from SanDisk and a few other brands ...Yes a few don't work but the speed is only a part of the problem.

    My advice is the same as many others buy one find it works ...stick with it.

     

    Also if you are having problems from the start  I would also make sure to use the writing program under windows which has a verify or have a Block Size (BS=128k) or similar using DD under Linux so that the writing speed is kept reasonable