Raspberry Pi Forum What is the maximum class memory Pi can support.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 685 subscribers
  • Views 959 views
  • Users 0 members are here
  • memory
Related

What is the maximum class memory Pi can support.

Former Member
Former Member over 11 years ago

I have heard Class 4 is the max but I have also heard that for audio must be Class 10 or better.

I found a link and its a bit sketchy as I found discrepant rating on the same SanDisk product I am attempting to use 32 class10 also look slike not all OS's are equal here

RPi SD cards - eLinux.org

Is there an optimal "chip" that supports the most OS's and runs fast Is the Proper Question.

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    0 Gough Lui over 11 years ago

    If I have one recommendation, it's to stay away from the Samsung Plus (Quick Review: Samsung Plus 32Gb UHS-I microSDHC Card | Gough's Tech Zone) and Samsung Evo (Quick Review: Samsung Evo 32Gb (MB-MP32D) microSDHC Card | Gough's Tech Zone) cards.

     

    For some reason, I've had many compatibility issues with them when it comes to heavy filesystem access causing I/O failures.

     

    Other than that, I've leveraged Sony, Toshiba, Sandisk regular/Ultra/Extreme, Kingmax cards with no failures to date. I've got over 6 Raspberry Pis and most of them run Class 10/UHS-I cards just fine. The Raspberry Pi doesn't seem to be able to take advantage of higher rates than ~22.5MB/s (i.e. DDR 25Mhz transfer mode), so UHS-I cards won't be fully taken advantage of.

     

    Another consideration is the type of I/O you're doing with the cards. As I've found through copious testing of cards with CrystalDiskMark, the cards will vary significantly - SD/SDHC/SDXC Performance Test Database | Gough's Tech Zone. The downside of this is that the faster Class 10 cards may be faster at large file sequential accesses, but be dog slow on small-file accesses. For things like updating or booting the OS, small file accesses are much more important than large file accesses. However, if you're streaming media or making a small personal NAS, then sequential speeds can be useful, although noting the Raspberry Pi won't go faster than about 22.5Mb/s because of its SD interface limits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 11 years ago

    If I have one recommendation, it's to stay away from the Samsung Plus (Quick Review: Samsung Plus 32Gb UHS-I microSDHC Card | Gough's Tech Zone) and Samsung Evo (Quick Review: Samsung Evo 32Gb (MB-MP32D) microSDHC Card | Gough's Tech Zone) cards.

     

    For some reason, I've had many compatibility issues with them when it comes to heavy filesystem access causing I/O failures.

     

    Other than that, I've leveraged Sony, Toshiba, Sandisk regular/Ultra/Extreme, Kingmax cards with no failures to date. I've got over 6 Raspberry Pis and most of them run Class 10/UHS-I cards just fine. The Raspberry Pi doesn't seem to be able to take advantage of higher rates than ~22.5MB/s (i.e. DDR 25Mhz transfer mode), so UHS-I cards won't be fully taken advantage of.

     

    Another consideration is the type of I/O you're doing with the cards. As I've found through copious testing of cards with CrystalDiskMark, the cards will vary significantly - SD/SDHC/SDXC Performance Test Database | Gough's Tech Zone. The downside of this is that the faster Class 10 cards may be faster at large file sequential accesses, but be dog slow on small-file accesses. For things like updating or booting the OS, small file accesses are much more important than large file accesses. However, if you're streaming media or making a small personal NAS, then sequential speeds can be useful, although noting the Raspberry Pi won't go faster than about 22.5Mb/s because of its SD interface limits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer