Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Regarding interfacing the chipkit pi to the raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 674 subscribers
  • Views 356 views
  • Users 0 members are here
  • spi
  • raspberry_pi
  • chipkit_pi
  • raspeberry_pi_accessories
Related

Regarding interfacing the chipkit pi to the raspberry pi

Former Member
Former Member over 10 years ago

Regarding interfacing the chipkit pi to the raspberry pi:

I'm sorry to be asking such a basic question, but as a newbie I simply can't find the answer.

 

One form of the question is -

what is the output voltage asserted on the Chipkit pi GPIO pins? Is it 5v0 or 3v3?   And does it depend on whether or not the chipkit pi is powered from the Raspberry pi or is separately powered?

 

Another way (I hope, otherwise I'm lost) of asking an equivalent question is:

Is it electrically safe to connect the SPI pins on the chipkit's "Raspberry Pi breakout header" (pins 16, 18, 20 on J4) to the corresponding pins on the chipkit's "Digital/Serial Header" (pins 7, 9, 11 on JA1)?

 

And if not what circuitry is needed to allow the Rasperry Pi to safely read SPI signals (or indeed GPIO signals) sourced by the chipkit pi? Would a simple zener to drop a 5v0 signal to 3v3 be sufficient given the low power involved?

Or how about a couple of forward biased LEDs in series to drop 5v0 to 2v6?  Using a 74LVC245 seems like overkill if it is not actually needed.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    The micro/IO rails on the Chipkit Pi is powered from 3.3V, so it can directly interface to the Pi.  There's a 5V to 3.3V regulator on the board to power the PIC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    The micro/IO rails on the Chipkit Pi is powered from 3.3V, so it can directly interface to the Pi.  There's a 5V to 3.3V regulator on the board to power the PIC.