Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Strange screen artifact
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 712 subscribers
  • Views 3753 views
  • Users 0 members are here
  • raspberrypi
Related

Strange screen artifact

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have 3 Pies

#1  1x Model B with 2 USB ports

#2  1x Model B+ with 4 USB ports

#4  1x Pi2  (there is only one model, right?)

 

I have used all 3 to run Openelec.

#1 works perfectly

#2 and #3 also run openelec but they both show an artifact on the top right-hand corner. It seems to be a miniature version of the colour screen that is shown right after the Pi wakes up but before it runs an OS.

 

Has anyone else seen this????

 

Cheers,

Nick

image

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 11 years ago

    Yeah. I've seen this...

     

    I take this logo to mean: "<something> is running" where "<something>" is probably something "videocore", the same thing that does the big square on boot up....

     

    My media center runs on an older 'pi, i.e. your "#1"....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to rew

    Hi Roger,

     

    Which models did you see this on?

    The weird thing is that this is done in both OpenElec and XBian. It almost feels like the firmware did not configure something correctly.

     

    I understand that the initial colourful screen is 4 actual pixels exploded by the GPU to fill the screen.

    The 'logo' I see looks like the GPU has then kept those 4 pixels on but at a smaller magnification factor....weird

     

    Cheers,

    Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to rew

    Hi Roger,

     

    Which models did you see this on?

    The weird thing is that this is done in both OpenElec and XBian. It almost feels like the firmware did not configure something correctly.

     

    I understand that the initial colourful screen is 4 actual pixels exploded by the GPU to fill the screen.

    The 'logo' I see looks like the GPU has then kept those 4 pixels on but at a smaller magnification factor....weird

     

    Cheers,

    Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rew
    0 rew over 11 years ago in reply to e14 Contributor

    I'm not "testing pi's if they work as a media center". I'm just "using a pi as a media center". The one I ended up with is the old B (no +). So I have only tested this with one pi, I've seen the square, thought: Hmm. apparently an indication that the GPU is running and forgot about it. It doesn't bother me.

     

    Yes, it looks as if the four pixels are painted and interpolated, for the startup screen blown up to almost fill the screen, while running openelec blown up to say 32x32 pixels or maybe 16x16.

     

    I would think it was put in as a debugging aid to see if the videocore processor is "up and running", it could have been taken out before "shipping" the software, but wasn't. Whether that was intentional or not I don't know.