I have a friend that's attempting to use OpenCV in a project on the RPi2. Has anyone worked with this, on the RPi2? If so, are there shortcomings?
Thanks a head of time,
Tim
I have a friend that's attempting to use OpenCV in a project on the RPi2. Has anyone worked with this, on the RPi2? If so, are there shortcomings?
Thanks a head of time,
Tim
I know has been working with OpenCV on the Raspberry Pi. The framerate on the B+ / Compute wasn't very good, ultimately, but on the Pi 2 it should be notably better.
You may find it easier to use the Python libraries rather than C or C++, depending on your skillset.
Heya Tim,
I haven't yet tried OpenCV on Pi2, I'll try it tonight. Have you got it working on any Raspberry Pi yet? it was a bit slow on the Compute for me but I was using both camera inputs and had a very inefficient algorithm doing the live video editing. So hopefully the Pi2 could be smooth even when using the python libraries, but you'll need to test that.
Heya Tim,
I haven't yet tried OpenCV on Pi2, I'll try it tonight. Have you got it working on any Raspberry Pi yet? it was a bit slow on the Compute for me but I was using both camera inputs and had a very inefficient algorithm doing the live video editing. So hopefully the Pi2 could be smooth even when using the python libraries, but you'll need to test that.
Callum,
Thanks for responding. Sadly, I don't yet have a RPi2 yet. I do have a CubieTruck and a RIoTboard that I can try it on. The Cubietruck is probably the closest thing that I have to the RPi2 (it's a multi-core A7 chip). Friend wants to use OpenCV to monitor a child, I'd like to attempt gesture recognition with it, hopefully without getting into too much coding. I'll keep notes on whatever I get working.
- Tim
Tim
The only problem that I can even imagine that you might have is if the drivers have changed when Raspbian got updated for the Pi2. The actual hardware shouldn't matter. So if you download the current Raspbian OS onto a micro SD card you could try it on another Pi and then it should work when you get your Pi2.
Callum
Callum,
Thanks!
- Tim