Raspberry Pi Forum Pi Appears to be working but no video.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 682 subscribers
  • Views 1461 views
  • Users 0 members are here
  • raspberry_pi
Related

Pi Appears to be working but no video.

Former Member
Former Member over 10 years ago

Hi my name is Jeff,

 

My new Raspberry Pi 2 Model B with 1 Gig of RAM recently arrived.

 

I attached a keyboard, mouse and ethernet cable. I know the mouse and keyboard work because I've tested them on a PC as well as my other Raspbery pi. (my other pi is the old b model with 512 MB RAM and seperate audio/video etc)

 

I don't have a HDMI tv so I then Plugged in a wv735 universal lead with a 3.5mm stereo Jack plug on one end and 3 RCA plugs on the other end into the Combined 3.5mm audio jack and composite video outlet.

 

I then plugged in a micro-sd card (tried a 4Gig card and a 16G card) I know both cards were working because I tried them in PC and my other Pi.

 

I used both NOOBS and raspbian as the OS on the Micro-SD card. I downloaded the most up to date versions from

 

Downloads | Raspberry Pi

 

I then proceeded to write it onto the Micro-SD card using the relevant instructions for the OS I used.

 

I then plugged in a micro-sd card into the pi (tried a 4Gig card and a 16G card just in case available memory was the issue) I know both cards were working because I tried them in PC and my other Pi.

 

Next I plugged in the power supply which is a switching adapter, Model : HNP10l-Micro USB

Input = 100-240v , 50/60Hz , 45A

Output = 5.0v , 2000mA

The following link is to a page containing a better description of what I have.

 

http://www.adafruit.com/product/1995

 

The power supply should be good enough to use since it is the same type I use on my other pi.

 

When power plugged in:

Red and greed lights came on

Red stayed on and green flashed a little bit (don't know how long) before turning off

Red light stayed on

 

When I pressed number 3 or number 4 the green light came on momentarily however the TV screen remained blank.

 

The only time I got anything on the screen is when I started to take the 3.5 mm jack out but never an image you could properly see.

 

Everything seems to work fine as far as I can tell but I can't get audio/video to work. I'm assuming it's a cable problem but I'm not sure.

 

Please help me so I can actually use my new Pi.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    you can hold 3 (PAL) or 4 (NTSC) while booting to force composite, this needs to be pressed pretty much as soon as you power up the pi, don’t wait for the green light activity to stop, do it as you plug in the power

     

     

     

    this should force the PAL or NTSC depending on if you pressed 3 or 4

     

     

     

    A 4GB card will work but you will run out of room pretty quick so yes a 16GB is the better choice, also make sure it is the right kind, compatible and approved for use with the PI (Class 10 etc)

     

     

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    you can hold 3 (PAL) or 4 (NTSC) while booting to force composite, this needs to be pressed pretty much as soon as you power up the pi, don’t wait for the green light activity to stop, do it as you plug in the power

     

     

     

    this should force the PAL or NTSC depending on if you pressed 3 or 4

     

     

     

    A 4GB card will work but you will run out of room pretty quick so yes a 16GB is the better choice, also make sure it is the right kind, compatible and approved for use with the PI (Class 10 etc)

     

     

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    Thanks for the advice.

     

    I tried what you said.

    I did it twice, once while holding the number 3 and once while holding the number 4, unfortunately it did not work.