Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Audio line-in for Raspberry Pi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 705 subscribers
  • Views 8433 views
  • Users 0 members are here
  • raspberry_pi
Related

Audio line-in for Raspberry Pi?

e14 Contributor
e14 Contributor over 11 years ago

Hi all!

 

Ok, so after a long time of looking at this cool stuff and not being able to come up with anything to do with it, I've finally hit on a project which seems perfect for something like a Raspberry Pi, and am eager to order up stuff and get started, only to find out that I've apparently picked the one area that the Pi apparently just doesn't really do very well.

 

Brief summary:  I want to build something that takes a stereo line-level audio input, performs some digital processing on it, and feeds it back out as a stereo line-level output.  I don't need anything terribly fancy, just basic unamplified CD-quality analog stereo in/out..

 

So after reading a bit, I discover that the Pi onboard audio output isn't very good, and it's onboard audio input is, well, apparently there just isn't one.  Ok, fair enough, lots of people just suggest plugging in a USB audio adapter, which aren't hard to come by, and they don't cost a lot, so I look into getting one of those and discover that pretty much all of them only have mono mic inputs, no stereo line-in capability (I found a couple that did, but they cost as much as the Pi itself, and were about twice the physical size, and at that point I might as well just get a cheap mini-ITX motherboard with onboard audio).  I also looked at the HiFiBerry DAC, but despite being pretty pricey, as best I can tell it doesn't actually have any input capabilities at all (so is actually worse for my purpose than a $2 USB adapter).

 

At this point it looks like the one thing that might work is the Cirrus Logic card?  It really seems like overkill, and costs more than the Raspberry Pi itself(!), but at least it has a line-input jack..

 

Am I missing something, or is this really my only option?

 

Alternately, are there any other SBCs in the same general power/size/price ballpark to the Raspberry Pi which have better onboard audio capabilities I could look at?

  • Sign in to reply
  • Cancel
Parents
  • gpolder
    0 gpolder over 11 years ago

    Alex, did you have a look at the The specified item was not found.?

    That will have everything you need.

     

    I agree with Michael that the RPi is not a digital signal processing system as such, but simple things certainly can be done. Even software defined radio runs fine in the RPi.

    (The specified item was not found.)

     

    best,

    Gerrit

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bklein
    0 bklein over 11 years ago in reply to gpolder

    Full blown (not command line) SDR seems anything but easy on the RPi2.  I've Googled and not found anyone with a howto for something that works.  You end up getting visuals but audio stutters.  CPU cores overload. I did find a video on youtube where it seems to be working but no clue how.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bklein
    0 bklein over 11 years ago in reply to gpolder

    Full blown (not command line) SDR seems anything but easy on the RPi2.  I've Googled and not found anyone with a howto for something that works.  You end up getting visuals but audio stutters.  CPU cores overload. I did find a video on youtube where it seems to be working but no clue how.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Problemchild
    0 Problemchild over 11 years ago in reply to bklein

    The RTL TV dongles and USB Audio cards can make plausible input devices for SDR on the RPI or many other computers, but has you said it seems that the RPIs tend to lack the puff to do it all reliably .. Many  are now using ODROIDs and similar to do the S/W decoding for applications like ADSB etc