I bought a second pi last month.
It said the 8gb sd came with noobs.
I plugged it all in where the other pi was and it never booted, only the power light came on.
i feel like i don't know what the hell I'm doing now.
can someone help me?
I bought a second pi last month.
It said the 8gb sd came with noobs.
I plugged it all in where the other pi was and it never booted, only the power light came on.
i feel like i don't know what the hell I'm doing now.
can someone help me?
its a 5v power supply
i plugged the sd into the running pi and nothing happened
this makes me think it doesn't have noobs on the sd like i thought
Did the power supply come with it or did you buy it separately or have it laying around?
Sometimes amperage is an issue. Depending on the Pi model, it is generally recommended 1A-2A (older models need about 1A, newer models like the Pi 2 should get 2A).
Did the power supply come with it or did you buy it separately or have it laying around?
Sometimes amperage is an issue. Depending on the Pi model, it is generally recommended 1A-2A (older models need about 1A, newer models like the Pi 2 should get 2A).
It is odd that the green 'SD Drive' light does not light. If the Raspi uses a micro-SD card, make sure it is pushed in and locks into place. I know I made quite sure the first time by giving it a second push, which of course popped it back out!
I have found that my cheap USB self-powered hubs actually feed 5V back to the connected computer which will light the Raspi red power LED, but will not boot the Raspi.
Even if you have the wrong OS on the card, the green light should operate and you should get a 'rainbow square' on the screen. If the green LED operates, but there is nothing on the monitor, plug the card into a USB card interface in another computer, go to the boot partition (it's a FAT file system so any computer should do) open config.txt in a text editor and change the line,
#config_hdmi_boost=4
to
config_hdmi_boost=4
Finally, the power supply is not as important as people think. Quite a low powered device can work well.
The USB lead connecting the PSU to the microUSB power socket on the Raspi is very important. A lead much longer than one meter is almost certain to fail. Use a lead of 500 mm (half meter) or 250 mm (quarter meter) to be sure. A one meter cable should boot the Raspi up with nothing plugged into the 2 or 4 USB device ports. However, once the ports are in use, it may lead to lockups, loss of mouse and keyboard or other OS failures.
There is a short list of silly mistakes that can stop the Raspi booting. I have the complete list, if you need it. However, if you follow this check list, you might get up and running.
I have my fingers crossed for you.