Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi power supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 705 subscribers
  • Views 1194 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Raspberry Pi power supply

e14 Contributor
e14 Contributor over 11 years ago

Hello! As I am getting several Raspberry pies to set them in parallel computing, I am looking for an adequate power plug to USB port, a USB switcher and several USB to micro-USB wires to connect the Raspberry Pies to the USB switcher. All this fulfilling the 5V and 750-1500mA of the Raspberry Pi http://www.element14.com/community/community/raspberry-pi/raspberrypi2

I am looking for a solution to buying several of these PSU, RASPBERRY PI, 5V, 2A, MICRO USB INT and having a cumbersome power plug.

  • Sign in to reply
  • Cancel
  • element14support
    0 element14support over 11 years ago

    Hello cyrilattie

    Welcome to the element14 Community, I will move this over to the Raspberry Pi 2 area as it is a better fit.

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to element14support

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    How many Pi are you wanting power for? If there are more than just a few, an old computer ztx power supply can be used. In one of the Ben Heck shows he used it to power. Raspberry Pi • View topic - Using an ATX power supply

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • screamingtiger
    0 screamingtiger over 11 years ago in reply to element14support

    If I were going to power several, I would de-solder the micro USB and directly wire them all in parallel.  Then have 1 power source either from an AC adapter that is designed to output lots of amps, such as something from a 12V laptop, or I would use a PSU as Clem suggests.  An RPi2 pulls 4W so if you have 10 of them you need 40W of power, but I would recommend 60-80W to account for USB, network etc plus you don't want to push the PSU too hard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago

    Hi Cyril,

     

    As one option -  the 5V supply line is available on the 40-way header (on two of the pins), so your power supply can be directly connected to that if desired. You lose the polyfuse protection but that could be an external (off-board) device if really needed.

    Take a look here for an example where the 40-way header was used to power the RPI (at that URL scroll down to the "Additional Ideas" section - in this case it was a 5V supply generated from a DC-DC converter connected to a battery but the concept is the same).