Raspberry Pi Forum The "Raspbeery" Pi Project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 685 subscribers
  • Views 668 views
  • Users 0 members are here
  • raspbeery
  • keg
  • beer
Related

The "Raspbeery" Pi Project

Former Member
Former Member over 10 years ago

Hello everyone!

A few months back, myself and a friend of mine both purchased keg fridges. We both brew our own beer and quickly came to the realization that putting beer into kegs is definitely a lot easier and less time consuming than bottling beer. But then the other problems quickly arose, like how much beer was in that keg and how many pints have you poured, etc. Which led the to Raspbeery Pi Project.

 

The outline of the project is this:

1. Know how full the keg is at all times

2. Know how many pints have been poured

3. Know how cold the beer is

4. Have a graphical representation with touchscreen controls showing all the above info mounted on the tap or tower.

5. Know when someone has poured a beer without permission (I.e. The teenager that opened a previously sealed bootle of whiskey and claimed it wasn't him)

 

Having done a few projects with arduino I knew the arduino would not be able to do the graphical components I have in mind.

So I've turned my attention to the Raspberry Pi. I've got all the hardware ordered that I think I'm going to need except for the touchscreen. I can't decided whether I want to use a 3.5" or 4" screen. My original plan was to build a custom tap handle with the Pi and the touchscreen mounted inside it. But I'm not opposed to mounting it on the beer tower either.

 

I ordered a 1/2" flow valve to mount inline on the hose between the keg and the tap.

I also ordered waterproof temp sensor and a 2steel ball tilt switch. I'll leave the temp sensor in the body of the fridge and the tilt switch will be mounted in the tap handle.

 

I've also ordered a wifi adapter so that I can tweet when the tap has been pulled without permission. And the whole thing will be based off the Raspberry Pi A+ as it draws less power and is in the smaller form.

 

Now here is where I need help.

I have never done any graphical programming before and don't know anything about Python.

I can't seem to find any starting tutorials for graphical programming. That work the way I'm going to be using things. Everything seems to be backwards. As in press a touchscreen button and it turns on an LED, not pull handle and it starts to count how much beer is flowing And then tell me how much is left in the keg.

 

Can anyone direct me to the best program for making up a gui this type of project?

And what OS should I start with loading on to the Pi?

 

Any other comments and suggestions are welcome as well.

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Papa_Guido

        https://wiki.python.org/moin/PythonGraphApi using python on raspbian...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Thanks clem57

    I will spend some time and see if I can figure out what that link is trying to say. Keep in mind I am a noob with the Pi.

    Most of that seemed to go right over my head but I'll give it a shot and see if I can translate it into something I can use.

     

    I am a hardware guy. My programming skills are very limited. And this project is probably way over my head. But I'm willing to give it a try. But im going to need some help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Thanks clem57

    I will spend some time and see if I can figure out what that link is trying to say. Keep in mind I am a noob with the Pi.

    Most of that seemed to go right over my head but I'll give it a shot and see if I can translate it into something I can use.

     

    I am a hardware guy. My programming skills are very limited. And this project is probably way over my head. But I'm willing to give it a try. But im going to need some help.