Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry PI - QNX
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 7 answers
  • Subscribers 716 subscribers
  • Views 10812 views
  • Users 0 members are here
  • raspberry_pi
  • qnx
Related

Raspberry PI - QNX

varghese_a
varghese_a over 11 years ago

Hi,


Has any one tried porting QNX on Raspberry pi ?

 

I am planning to take it up atleast the Graphics (HDMI) & Network part.

 

Varghese

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Looks like after a few years of asking, no one has been very successful. Would love to know your results.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    There is a company that has done a port of QNX to Raspberry...

     

    http://swhwc.com/?lang=en

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    > do not see it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to clem57

    I thought at first it might be simply an advert, but some digging found this.

     

    http://swhwc.com/bussiness/products.html?lang=en

     

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to mcb1

    On the site intro they wrote:


    This is a very primitive BSP presently but capability can be expanded (to some degree) per user needs. Due to the lack of hardware manual from Broadcom, I heard no one wanted to develop QNX BSP for Raspberry Pi. Our Vietnamese engineer friends have gone through incredibly hard development without any hardware manual. They had to reverse engineer hardware spec from reference code. Now Broadcom and Avago merged we will see what happens to the documentation situation.


    Noticeable the reverse engineering of their guy but if by one side there is no hardware info by the other there is - at least, but I think can be found more - a whole bunch of different linux versions running on the PI. Why not to take a look on how these distro works, plus the sources (opensource) libraries to manage the various hardware features, GPIO and so on instead of risking to become crazy with a hardware exploitation ?

    It's just a doubt.


    Enrico


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to balearicdynamics

    Well spotted.

    I just went to see if it was there. I have no use for it but the original OP might ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to mcb1

    In past I have rebuilt a Ubuntu linux OS inside a Android box with full system replacement (Android dismissed) and to be honest, never opened this stuff image , then refactored a tablet with Ubuntu swappable with Android and never opened it image

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to balearicdynamics

    I'm not sure why they say there is no hardware manual as there has been one out for all the SoC peripherals (except USB) for a couple of years now and one for the GPU for at least a year now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • varghese_a
    0 varghese_a over 11 years ago in reply to gdstew

    After some research I found ,

     

    It is possible to Make QNX porting for Raspberry PI .. The documents available in the public domain are more than sufficient ..

    I have got a hobbyist license for QNX6.5.0  . 

     

    My attention got diverted towards WinCE( Got dreamspark licence for wince 7) ,as there is a partial porting already available & I got extensive experience on Windows based systems .https://ceonpi.codeplex.com/   .dboling did a wonderful job..  He has finished the kernel startup/serial & graphics support..  He got struck with USB ...


    I tested it using Rasperry B+ module, its working well .. Since there is No usb support ,we cant feed any input to the OS.. So I added some application in the startup OS routine to turn ON LEDs , It is working well ..


    I am adding the USB support , just half way through ... once it is done ,i will put the code in Github..

    For those who are interested..  here is the method ..  we can add usb driver  support in 2 ways ..

     

    1. USB bare metal code is available here   https://github.com/Chadderz121/csud

    By exploiting the USB stack , we can just get the mouse & keypad data and using that data we can simulate the window events (mouse movements /key press)... Kind of PS/2 keyboard mouse , but still it will use USB port.  I know , it  is a bad way of coding , but the advantage is, time will be greatly saved ...  No coding required image

     

    2.Other method is tinkering the  (ochi/echi/uhci/) code & making it work with Designware stack  .. It is the best method , because once usb stack is UP , keypad ,mouse ,touch , pen drive ,LAN everything will work automatically ..

     

    Parallely I am going to work on QNX too ..

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gdstew
    0 gdstew over 11 years ago in reply to varghese_a

    Great, I thought so! I would love to experiment with QNX but needing a license gets in the way. If the source is available you might want to take a look at the Linux USB driver

    as it has been highly tuned to get decent full USB host performance out of the USB OTG hardware.

     

    I have considered porting a couple of Linux kernel real-time patch sets such as RTAI (Real Time Application Interface) or Xenomai but they tend to be well behind kernel

    development so finding a recent kernel compatible version is a problem and I just can't find time to do it. I still haven't heard much of anything good about the official Linux

    kernel real time patches.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 11 years ago in reply to varghese_a

    Great, I thought so! I would love to experiment with QNX but needing a license gets in the way. If the source is available you might want to take a look at the Linux USB driver

    as it has been highly tuned to get decent full USB host performance out of the USB OTG hardware.

     

    I have considered porting a couple of Linux kernel real-time patch sets such as RTAI (Real Time Application Interface) or Xenomai but they tend to be well behind kernel

    development so finding a recent kernel compatible version is a problem and I just can't find time to do it. I still haven't heard much of anything good about the official Linux

    kernel real time patches.