Raspberry Pi Forum Enable the IT9135 (WandTv) DVB Usb stick
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 686 subscribers
  • Views 4903 views
  • Users 0 members are here
  • raspberry_pi
Related

Enable the IT9135 (WandTv) DVB Usb stick

Former Member
Former Member over 10 years ago

Dear friends,

 

I tried to ask in many forums (without any success) regarding the use of the WandTv DVB stick on Raspberry PI 2 with any XBMC (Kodi) flavor.

 

Does anyone knows how to do that in a simple way?

 

I'm a newbie without much knowledge on Linux, neither programming.

 

Thank you very much!

 

Ilan.

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    Do you have Rasbian? If so, open a terminal window and try the command with the DVB plugged in:

    lsusb

    The output will tell me what drivers you need.

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Dear Clem,

     

    It tells me that the command is not found...

     

     

    https://dl.pushbulletusercontent.com/xfC6gK7snCboSPdHfQp2Sq3LhnplSnSK/20150416_222201.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    "dmesg" for the messages will provide the same information. But warning it may be a lot. "lsusb" in lowercase did not work? try "uname -a".

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Dear Clem,

     

    I did dmesg and have it on a text file here:

     

    https://www.dropbox.com/s/fi5bgmvee7yyw42/clem.txt?dl=0

     

    Unfortunately isusb did not work (I reinstalled raspbian)

     

     

    p.s. I know that the WandTv use the IT9135 chip.

    I also know that there are Linux drivers (on the installation CD) but I don't know how to make it work on OSMC or Xbian.

     

    Thank you,

     

    Ilan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dtsartsanis
    0 dtsartsanis over 10 years ago in reply to Former Member

    http://forum.osmc.tv/printthread.php?tid=2912

     

    http://www.linuxtv.org/wiki/index.php/ITE_IT9135

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Try these first:

     

    3. The device manager udev will "automagically" create appropriate device nodes on /dev:
    (a) For a DVB device, you should now have a non-empty /dev/dvb directory. You can check on whether this is true for you with the following command:

    ls -l /dev/dvb/

    (alternatively, you can browse your directory structure with the graphical file manager of your choice). If you have a single DVB device installed in your system, then the output of the above command should reveal that /dev/dvb/ is populated by adapter0. Digging further,

    ls -l /dev/dvb/adapter0

    reveals the character devices associated with adapter0 for which the drivers have control. If you have more then one DVB device, you can see the same for all with

    ls -l /dev/dvb/adapter*

    (b) For a V4L device, you should now have a non-empty /dev/v4l directory. You can check on whether this is true for you with the following command:

    ls -l /dev/v4l

    Digging further,

    ls -l /dev/v4l/by-path

    reveals the symbolic links to the character devices associated with your V4L adapter for which the drivers have control. The most typical of which is /dev/video0. If you have more then one V4L device, you can see the same for all with

    ls -l /dev/video*

     

     

    By the messages, I believe the following will help you install the drivers if needed.

    How to Obtain, Build and Install V4L-DVB Device Drivers - LinuxTVWiki

    Let me know if this helps by marking this entry as correct, otherwise drop more information...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to dtsartsanis

    Dear Dimitrios,

     

    The post you sent me is from 2012.

    After reading, even on the second link, it says that on the new kernels, there is no need to do that procedure.

     

    Maybe I miss something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Dear Clem,

     

    Thank you for your answer.

    The problem is that this is a bit complicated to me to compile drivers in Ubuntu (or maybe Raspian).

     

    I'm sure that many users do use some kind of DVB stick with any kind of Kodi with Raspberry.

     

    Isn't a simple solution for that, with simple steps for Raspberry?

     

    Thank you again!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Dear friends,

     

    Now I am completely lost!

     

    I tried to follow the tutorial of Dimitrios on

    [HowTo] Raspbmc PVR TinyUSB2 DVB-T & TVHeadend All-in-one - Printable Version

    Now, after I did this step:


    sudo -s

    cd /

    wget http://goo.gl/jFh9x -O rootfs.tar.gz

    tar -xzf rootfs.tar.gz

    cd /boot

    wget http://goo.gl/Xj3IR -O vfat.tar.gz

    tar -xzf vfat.tar.gz

    reboot


    My Raspberry Pi2 won't turn on.


    What can I do now?


    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to Former Member

    Although many "howto's" from 2012 are still valid, some of them are not. Late 2014 the raspberry pi 2 was introduced. As it has a different CPU, the firmware needed to be updated. So if you download and install firmware from 2012, it will not boot on your PI 2.


    I'm not sure where the "goo.gl" links point to, but if that hasn't been upgaded since that was written, your firmware is too old.

     

    To get it to boot again: Download NOOBS or something like that and start over.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>