Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Epitaxial vs 1N4002 Diodes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 28 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 4838 views
  • Users 0 members are here
  • epitaxial
  • diode
  • ethernet
  • lan
  • network
  • raspberry_pi
  • connection
  • prototyping
  • raspberrypi
  • lan-hub
Related

Epitaxial vs 1N4002 Diodes

balearicdynamics
balearicdynamics over 11 years ago

Someone knows if it is acceptable to use diodes of the type 1N4001 or 1N4002 instead of epitaxial diode to manage signal channels with levels and frequencies of the order of the Ethernet 10/100 ? I have never used the Epitaxial pin diodes and I have no idea.

 

Thanks in advance, any suggestion is welcome image

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago
    • SP3002 0.85pF, 12kV, Low Capacitance Diode Array for ESD Protection  should work for ESD protection...

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to clem57

    Many thanks, Clem.

     

    In the meantime after a reasonable investigation on the use I had in mind it seems that it is not the better solution. I was exploring the possibility to have a passive hub but it is not so reliable and - worst of all - it seems that with the LAN works only in half-duplex. The best usage seems to be with TV signals integration but it is not my case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to michaelkellett

    Agree with you on all points there.

    Need to know what sort of project he is taking on to give some idea of required speed and acceptable latency!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to Problemchild

    Sorry for the delay in my answers, I have read all your last comments on the mobile that is not very good to write decent responses.

     

    John, the problem is not the cost as I already have one to make tests. The speed of 10/100 is more than sufficient. Your answer and the other guys before already gives me the correct vision, despite the project itself, that the choice now is between ISP (that is the less valuable I think) and the LAN connection that it is very probably I will decide for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to michaelkellett

    Michael, as you wrote

     

    1) The whole idea is pretty dreadful since it relies on undocumented and unintended behavior of of the 10baseT or 100baseT hardware - however it obviously could work in some setups.

    2) The diodes will need to be fast - 1N4002 would not work, 1N4148s probably would.

    3) You can buy a 5 port switch from Amazon for £5.86 - you won't be able to buy one switch chip and the connectors for this price so building your own switch would be mad.

    1) That's ok, I have explored again the of the passive hub (mostly for the power consumption but it is unreliable for too much aspects, so it is excluded apriori

    2) This is anyway an information that I need at least for curiosity; following simply the logic, if there are specific high speed diodes there would be a reason, and this is another point that address me to exclude the solution.

    3) That's ok for the mini switch and the problem is not the price itself


    The project is - in general - metitech_project (this is the tag, you can find all the already wrote posts in the SiFi your Raspberry-Pi challenge blog). In this moment I am focusing all the obscure points, ad this is one of them, to define the complete architecture of the system.

     

    For several reasons I have to use more than one RPI and I should have them exchanging data together in a private internal connection. Then at least two units will be in the same "box" or container. The system in general will be modular so some complex probes - better group of probes - will be external pluggable components driven by another RPI. The same mobile lightweight box will be also available in  a non-portable version with the devices connected together via a network. The "main controller" RPI will include a wifi for the main interface (Android based) so with these premises I think that the LAN is revealing to be the right solution.

     

    The doubt that I already have is about the suggestion os clem57 about the possibility to use for the internal connections the SPI protocol. As I wrote in a precedent post, if by one side the SPI protocol on RPI has the limitation that doesn't support the slave mode by the other there is the master to master connection that - as for what I have read - seems to use only one channel instead of the traditional two bidirectional wire lines MISO and MOSI.

     

    Anyway a t the moment I am strongly prepending for the LAN also for the internal connections.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to balearicdynamics

    Hello Enrico,

     

    Now I know about your project I would definitely use LAN for communications. The advantages of SPI would not be available to you in this context. The implementation of Ethernet on the Pi is far from ideal but will probably be OK (I'm assuming that the earlier reliability issues have been sorted out  - some RPI expert may have  a comment here.)

     

    One big advantage of using Ethernet is that the integration with Linux is far better than for any other reasonable bandwidth communications available to you on a PI.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to balearicdynamics

    The spi can work if each RPI is a master and say an Arduino is the slave. One extra line is needed to send interrupt from Arduino back to a  particular RPI to request he master the bus high for a transfer back to him. Also before a master uses the bus, he must interrogate the bus in use because the select is already high (someone else using).

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 10 years ago in reply to balearicdynamics

    balearicdynamics Ciao Enrico whats up? I have been working hard to have a new tidbit to show off at Cockpit-Fest at the end of the month. image

    I Finally got the damn Pearl translated and updated in C. I spread it out over 6 modules... with the six header files a well. The update is to fix

    the Pearl global variables ie make them local and use C structures to hold the data. makes life better. and my buddy Paul to stop bitching about Pearl.

    No food to brag about but I just make some "Home Fries". Take some reds and nuke them for about 6min. cut them up to about 1"/30mmSQ Then toss themimage

    into a nice frying pan, add Green Peppers, Onions, Course Ground Black Pepper, and a *** Load of Garlic, and Chives optional .  Can also do in oven.

    cook medium heat, the object is to brown the spuds., then of course some bacon and eggs..image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 10 years ago in reply to balearicdynamics

    hey its me again, yes but no, your wired ethernet LAN is Full Duplex, with a switch, yes you can force it in to a HD mode but why?

    What Is Half-Duplex And Full-Duplex Operation, And How Does It Affect Your Router?

     

    Later

    Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to phoenixcomm

    Hi phoenixcomm Cristina ! I am fine. Always raining here but lot of projects are going ahead... And as in the Netherlands it seems they have no idea on how to cook anything else then deep-fry stuff, I made great progresses with my personal variations of receipts.

     

    See you your potatoes seems really nice. I love this kind of cooking.

     

    Cheers, Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 10 years ago in reply to balearicdynamics

    balearicdynamics, Enrico, What drugs are to taking, from Meditek thing??? Enrico, you are smarter than this, I thought. Building an e-net hub is crazy.  The diodes are the least of the problem, Remember you need Magnetics as well.

    Please go get a WRT-54G and remove its case.  The switches are very robust. you will have more than double the throughput  as 10Bt was never FD only HD.

    Plus you will have a 100 Mb backplane as well and you don't have, Plus another factor 10Mb to 100Mb good jump there as well. Oh yes, I almost forgot network collisions and retransmits, POFF, NONE, GONE

    his is a specialized processor, don't think the pie could deal with this.

    Cris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to phoenixcomm

    phoenixcomm Hi dear phoenix image you are correct. Most of the parts of the first Meditech project was just a proof of concept and the next prototype (the one on the road for the product) will be reviewed in some strategical parts. I will publish more about this at the end of August. And the software too will be revised. And also this part will be notices further for some reasons. Contact me pvt for some preview news if you are interested.

     

    BTW, I have thenused a hacked hub for this solution.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to phoenixcomm

    phoenixcomm Hi dear phoenix image you are correct. Most of the parts of the first Meditech project was just a proof of concept and the next prototype (the one on the road for the product) will be reviewed in some strategical parts. I will publish more about this at the end of August. And the software too will be revised. And also this part will be notices further for some reasons. Contact me pvt for some preview news if you are interested.

     

    BTW, I have thenused a hacked hub for this solution.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 10 years ago in reply to balearicdynamics

    enrico_miglino That a way to go!! Knew you it in you!!image

     

    Cris H.