Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum RPI Network working but no internet
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 704 subscribers
  • Views 5919 views
  • Users 0 members are here
  • pi_networking
Related

RPI Network working but no internet

e14 Contributor
e14 Contributor over 11 years ago

My Pi won't connect to the internet. Everything was fine until my TalkTalk Huawei router died and I replaced it with a TP-Link TL-WR841ND. Now the networking is OK but no internet.

 

The Pi gets it's IP settings at boot time through 'ip=dhcp' in cmdline.txt from the WR841. It is a reserved address on the router so it always gets the same, 10.96.19.99 (as was with the Huawei). There are no IP conflicts on the network.

That works fine. The Pi boots over the network from a share on my NAS drive - that also works without problem.

I can access all of the shared resources on my network, NAS shares, printers etc.

The various PCs, Xbox, tablets and smart phones in the house, some of which are WiFi others are hard wired, have total internet access, no problem.

Now it gets weird; I can connect to the configuration pages on the router from the Pi but it is so desperately slow it's unreal. Perhaps two minutes to make the connection then probably the same for each page. It's almost instantaneous from a PC.

And, of course, no internet access whatsoever. apt-get fails to find the various archive sites and none of the browsers I have loaded will access web pages not on my network. Web pages on the network all appear to suffer the same speed issues as WR841.

The only thing I have noticed that I don't quite understand is that it has registered the router as a name server, which it isn't but then I access the local web pages by ip address rather than by name so it shouldn't need to look for a name server.

 

Does anyone out there have any bright ideas about what may be going on. I'm stumped!!!

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Please do the following test and post output here:

    ifconfig

    ping 10.96.19.99

    ping 8.8.8.8


    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    It's a bit messy but here are the results. Pinged the router too for good measure.

    What's 8.8.8.8? that's a new one on me.

     

     

    ifconfig

     

    eth0 Link encap:Ethernet HWaddr b8:27:eb:6c:3b:7f

     

    inet addr:10.96.19.99 Bcast:10.96.19.255 Mask:255.255.255.0

     

    UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1

     

    RX packets:173729 errors:0 dropped:18 overruns:0 frame:0

     

    TX packets:115202 errors:0 dropped:0 overruns:0 carrier:0

     

    collisions:0 txqueuelen:1000

     

    RX bytes:171502110 (163.5 MiB) TX bytes:61690306 (58.8 MiB)

     

    lo Link encap:Local Loopback

     

    inet addr:127.0.0.1 Mask:255.0.0.0

     

    UP LOOPBACK RUNNING MTU:65536 Metric:1

     

    RX packets:1506 errors:0 dropped:0 overruns:0 frame:0

     

    TX packets:1506 errors:0 dropped:0 overruns:0 carrier:0

     

    collisions:0 txqueuelen:0

     

    RX bytes:112928 (110.2 KiB) TX bytes:112928 (110.2 KiB)

     

     

     

     

    PING 10.96.19.99 (10.96.19.99) 56(84) bytes of data.

     

    64 bytes from 10.96.19.99: icmp_req=1 ttl=64 time=0.177 ms

     

    64 bytes from 10.96.19.99: icmp_req=2 ttl=64 time=0.142 ms

     

    64 bytes from 10.96.19.99: icmp_req=3 ttl=64 time=0.147 ms

     

    64 bytes from 10.96.19.99: icmp_req=4 ttl=64 time=0.152 ms

     

    64 bytes from 10.96.19.99: icmp_req=5 ttl=64 time=0.145 ms

     

    64 bytes from 10.96.19.99: icmp_req=6 ttl=64 time=0.146 ms

     

    --- 10.96.19.99 ping statistics ---

     

    6 packets transmitted, 6 received, 0% packet loss, time 4995ms

     

    rtt min/avg/max/mdev = 0.142/0.151/0.177/0.017 ms

     

     

     

    PING 10.96.19.102 (10.96.19.102) 56(84) bytes of data.

     

    64 bytes from 10.96.19.102: icmp_req=1 ttl=64 time=3.79 ms

     

    64 bytes from 10.96.19.102: icmp_req=2 ttl=64 time=0.548 ms

     

    64 bytes from 10.96.19.102: icmp_req=3 ttl=64 time=0.528 ms

     

    64 bytes from 10.96.19.102: icmp_req=4 ttl=64 time=0.532 ms

     

    64 bytes from 10.96.19.102: icmp_req=5 ttl=64 time=0.545 ms

     

    64 bytes from 10.96.19.102: icmp_req=6 ttl=64 time=0.626 ms

     

    --- 10.96.19.102 ping statistics ---

     

    6 packets transmitted, 6 received, 0% packet loss, time 4999ms

     

    rtt min/avg/max/mdev = 0.528/1.094/3.790/1.206 ms

     

     

     

    PING 8.8.8.8 (8.8.8.8) 56(84) bytes of data.

     

    64 bytes from 8.8.8.8: icmp_req=1 ttl=53 time=16.5 ms

     

    64 bytes from 8.8.8.8: icmp_req=2 ttl=53 time=15.5 ms

     

    64 bytes from 8.8.8.8: icmp_req=3 ttl=53 time=16.9 ms

     

    64 bytes from 8.8.8.8: icmp_req=4 ttl=53 time=15.6 ms

     

    64 bytes from 8.8.8.8: icmp_req=5 ttl=53 time=16.2 ms

     

    --- 8.8.8.8 ping statistics ---

     

    5 packets transmitted, 5 received, 0% packet loss, time 4003ms

     

    rtt min/avg/max/mdev = 15.570/16.214/16.940/0.539 ms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Ahhh. Google public DNS. So something's getting out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Yes you are right. What I would suggest is forcing the DNS address to 8.8.8.8 for nameserver. Looking at http://www.heystephenwood.com/2013/06/use-your-raspberry-pi-as-dns-cache-to.html, we have a problem of DNS right now.

    So do:

     

    Enter the following command to edit the resolv.conf file.

    sudo nano /etc/resolv.conf

    Enter the follow Google public dns server IP address.

    nameserver 8.8.8.8
    nameserver 8.8.4.4

    Press CTRL-X to exit but remember to save the file by accepting the changes.

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Yes you are right. What I would suggest is forcing the DNS address to 8.8.8.8 for nameserver. Looking at http://www.heystephenwood.com/2013/06/use-your-raspberry-pi-as-dns-cache-to.html, we have a problem of DNS right now.

    So do:

     

    Enter the following command to edit the resolv.conf file.

    sudo nano /etc/resolv.conf

    Enter the follow Google public dns server IP address.

    nameserver 8.8.8.8
    nameserver 8.8.4.4

    Press CTRL-X to exit but remember to save the file by accepting the changes.

     

    Clem