Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How can I set the SPDIF Out of a Wolfson card for 48KHz output
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 706 subscribers
  • Views 1173 views
  • Users 0 members are here
  • wolfson
  • audio
  • raspberry_pi
  • raspberry-pi
  • raspeberry_pi_accessories
Related

How can I set the SPDIF Out of a Wolfson card for 48KHz output

e14 Contributor
e14 Contributor over 11 years ago

Just registered and after a long research...

 

The set:

  • Wolfson card on Raspberry Pi B
  • Volumio 1.55 with the patch of Ragnar
  • Yamaha RX-V595RDS
  • very cheap cinch auido cable, about 1.5m (for sure not a chance to be 75 Ohm)
  • some mp3, FLAC files

 

The history:

  • Headset out: OK
  • Line-out: OK
  • SPDIF Out: the receiver complains with "data error"
  • CD-Player with a coaxial cable (the very cheap one): OK (SPDIF)

 

The specs:

  • Yamaha RX-V595RDS has input rate 48Khz, 16 bit (or 24, not sure)
  • Wolfson SPDIF output: ?? (192KHz maybe? or depends on the bitrate of the file?)

 

I suppose that the problem should be the incompability between the Wolfson SPDIF and the Yamaha RX-V595RDS input and in particular the rate too high... But it could be also wrong.

 

The question(s):

  • How can I set 48KHz rate on SPDIF out?
  • Could there be another reason for the "data error"

 

And any other suggestions (except for other than RaspberryPI/Wolfson card) are welcome, of course.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Looking at the protocol for the digital bits for SPDIF, there is a check for even/odd parity. Should this be wrong, a possible data error would occur.

    clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago

    Looking at the protocol for the digital bits for SPDIF, there is a check for even/odd parity. Should this be wrong, a possible data error would occur.

    clem