Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 A/V output via RCA Question.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 3 answers
  • Subscribers 708 subscribers
  • Views 14024 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 A/V output via RCA Question.

e14 Contributor
e14 Contributor over 11 years ago

I have the RP2 running RetroPie and have used it via HDMI.

 

I now want to use my 3.5mm to RCA cable. I have tried but get not picture. My TV seems to see something is there but I get no audio or video. I have made sure the yellow is in yellow, red to red, white to white and that the 3.5mm is firmly in the RP2.

 

The 3.5 mm jack has 3 black bands if that helps.

 

Any ideas?

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Does your pi side look like this?

    image

    The problem is 3 types. Only if GND on second ring will this work with Pi. Sometimes the video is not yellow, but red( or white). Try all other two and report which works.

    http://www.anythingbutipod.com/archives/images/av-pinouts.jpg

    If you have a camcorder cable then red is video

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    hello I m new user like you guys to lovely "Raspberry pi 2" ,

    i m like you faced the problem in getting output on tv using RCA VIDEO cable,but after some research found a complete solution,

    Solution to RCA VIDEO output prolem: Two steps

    Step 1:Hardware setup,i,e whatever the rca cable you have bought mostly have the yellow pin with connections in reverse as per Rapberry pi requirement ,

           so you the cut yellow wire at distance of 10 cm from male pin and reverse the connection with black to yellow and yellow to black, now you are fit with RCA hardware                         compatability.

    Step 2: If you connect Raspy to  tv powered on and then power on your raspy,if you dont see anything on tv (with AV screen on ,for which the Raspy has been connected)

              go for "config.txt" editing ,Add the folliwing lines of code, (note:if a line of code already exist dont repeat it)

            

     

     

    sdtv_mode=2

    hdmi_ignore_hotplug=1

    #hdmi_force_hotplug=1        

    #note above lines added to have composite display,and hdmi will not come,if you want hdmi display on,comment above two lines,and uncomment third line.

     

     

     

     

     

     

     

    i think i have given a quick solution for the problem of not having output on CRT TV using RCA Video cable .

    If your problem is solved please comment out,or for any queries.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    hello I m new user like you guys to lovely "Raspberry pi 2" ,

    i m like you faced the problem in getting output on tv using RCA VIDEO cable,but after some research found a complete solution,

    Solution to RCA VIDEO output prolem: Two steps

    Step 1:Hardware setup,i,e whatever the rca cable you have bought mostly have the yellow pin with connections in reverse as per Rapberry pi requirement ,

           so you the cut yellow wire at distance of 10 cm from male pin and reverse the connection with black to yellow and yellow to black, now you are fit with RCA hardware                         compatability.

    Step 2: If you connect Raspy to  tv powered on and then power on your raspy,if you dont see anything on tv (with AV screen on ,for which the Raspy has been connected)

              go for "config.txt" editing ,Add the folliwing lines of code, (note:if a line of code already exist dont repeat it)

            

     

     

    sdtv_mode=2

    hdmi_ignore_hotplug=1

    #hdmi_force_hotplug=1        

    #note above lines added to have composite display,and hdmi will not come,if you want hdmi display on,comment above two lines,and uncomment third line.

     

     

     

     

     

     

     

    i think i have given a quick solution for the problem of not having output on CRT TV using RCA Video cable .

    If your problem is solved please comment out,or for any queries.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer