Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 A/V output via RCA Question.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 3 answers
  • Subscribers 708 subscribers
  • Views 14181 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 A/V output via RCA Question.

e14 Contributor
e14 Contributor over 11 years ago

I have the RP2 running RetroPie and have used it via HDMI.

 

I now want to use my 3.5mm to RCA cable. I have tried but get not picture. My TV seems to see something is there but I get no audio or video. I have made sure the yellow is in yellow, red to red, white to white and that the 3.5mm is firmly in the RP2.

 

The 3.5 mm jack has 3 black bands if that helps.

 

Any ideas?

 

Thanks.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    but clem sir, i have already two 3.5mm stereo to 3 rca av cables but both are not supported. may be this is a same situation as kevin. video as yellow and it is gives some result but not pure.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    The cables are not all alike even though they have 4 rings on tip:

    image

    Check yours in diagram above to correct above.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    thanks sir, that means i will change my cable's stereo pin connection..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • indianx
    0 indianx over 9 years ago in reply to clem57

    I had got the same  trouble with the pi2, got the solution with the option 4 as the ipod video it works great!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<