Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi camera Python3 interface issues
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 705 subscribers
  • Views 732 views
  • Users 0 members are here
  • pi_camera
  • raspberry_pi
Related

Pi camera Python3 interface issues

plmsherman
plmsherman over 11 years ago

I'm working on a project that uses a Pi camera that needs to be controlled through Python because I can't use auto exposure. The camera is working and creating images but there's three problems I've encountered that I can't resolve. All of the problems are dependent on a single function call of the camera setup

1. There's no preview image

2. Image capture takes almost 30 seconds

3. The zoom() function is disabled - I'd like to have this but it isn't a necessity

 

All of these problems appear to be results associated with the camera.framerate() call. If I remove it from the command set, the camera functions normally, with a preview screen and the image capture takes a fraction of a second. The zoom() function also works normally. With the framerate() call in the command set, there's no preview but there's a very short duration image on the display as the image is taken. Unfortunately, without the framerate() call, the exposure time is limited to 33ms. It also appears that almost all of the 30 second delay starts when the capture() call is issued and ends when the image appears on the screen.

 

I'm open to any suggestions as to how I can eliminate the long delay. Getting a preview image would be nice but isn't a necessity for this application.

 

Phil

 

Python camera control code:

 

with picamera.PiCamera() as camera:

    camera.resolution = (2582,1944)

    camera.framerate = Fraction(1,6)

#    camera.zoom = (0.25,0.25, 0.25,0.25)

    camera.shutter_speed =190000

    camera.iso = 800

    camera.start_preview()

    time.sleep(5)

    camera.capture(my_file)

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago

    I am willing to bet the issue is in the camera object code. Have you taken a look inside?

    Clem

    Edit:

    Please open an "Issue"  at https://github.com/waveform80/picamera for the developer. Add as much details as you can so that it can be resolved quickly.

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • plmsherman
    0 plmsherman over 11 years ago in reply to clem57

    I'd like to but I'm getting under time pressure to complete the software I'm writing and won't have time to examine it. I expect to need at least another 100 hours to tie all pieces that are finished together then develop a GUI user interface for it.

     

    I'll take your recommendation and open an issue at github. Thanks for the reference to it.

     

     

    Phil