Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Music hosting idea. Is it possible?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 705 subscribers
  • Views 899 views
  • Users 0 members are here
  • raspberry_pi
Related

Music hosting idea. Is it possible?

e14 Contributor
e14 Contributor over 14 years ago
.
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    You can install MPD (music player daemon) on Raspbian. From the configuration file, you can enable an HTTPD stream as a type of audio output. Then you can just navigate to "http://YOURPUBLICIP:YOURPORT" in a browser or internet radio player to stream. Controls can be through any MPD client on any computer, Android device, etc. I usually SSH into a screen session running ncmpcpp to control, but MPDroid is a pretty good graphical client for Android. Furthermore, this service can be secured with a password easily. You just need to set a password directive in the MPD configuration file. That way, you will need a password to unlike the controls and/or the audio stream. You can also easily change the quality/bit-rate of the stream so that it's tailored perfectly to your connection. If you're streaming over the internet, the bitrate would have to be lower. However, if you're just streaming locally, you can set it up nice and high.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    You can install MPD (music player daemon) on Raspbian. From the configuration file, you can enable an HTTPD stream as a type of audio output. Then you can just navigate to "http://YOURPUBLICIP:YOURPORT" in a browser or internet radio player to stream. Controls can be through any MPD client on any computer, Android device, etc. I usually SSH into a screen session running ncmpcpp to control, but MPDroid is a pretty good graphical client for Android. Furthermore, this service can be secured with a password easily. You just need to set a password directive in the MPD configuration file. That way, you will need a password to unlike the controls and/or the audio stream. You can also easily change the quality/bit-rate of the stream so that it's tailored perfectly to your connection. If you're streaming over the internet, the bitrate would have to be lower. However, if you're just streaming locally, you can set it up nice and high.