Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Connect analog cctv to RPI 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 709 subscribers
  • Views 8495 views
  • Users 0 members are here
  • cctv
  • raspberry_pi
  • raspberrypi
  • analog
Related

Connect analog cctv to RPI 2

e14 Contributor
e14 Contributor over 10 years ago

I am working out for my project and I want to use my old Analog CCTV and connect it to RPI 2. Is it possible to connect the analog cctv to RPI pins without using any converter? Anybody who can help me with this?

 

I am a nube by the way and still don't know the tracks. But I want to learn and expand my horizon.

 

Thanks for the help in advance.

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    Problemchild over 10 years ago

    If you mean an old CCTV monitor then yes you can the output form the RPI is normal Composite video which will work fine in most CCTV setups.

    Obviously you will need to have a lead made up to connect the two but you should be OK.. Also make sure you set it to the local video standard weither that's PAL or NTSC.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 10 years ago

    If you mean an old CCTV monitor then yes you can the output form the RPI is normal Composite video which will work fine in most CCTV setups.

    Obviously you will need to have a lead made up to connect the two but you should be OK.. Also make sure you set it to the local video standard weither that's PAL or NTSC.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rew
    rew over 10 years ago in reply to Problemchild

    John it is the other way around. He wants to connect the CCTV camera on his raspberry pi.

     

    Dear Divina. The technically correct answer is: But of course you can connect your analog CCTV signal to your raspberry pi pins without any converter". The thing is, the 'pi is not equipped to process analog TV signals like your CCTV signal. it simply doesn't have the circuits to process the signal. So it won't be able to do anything with it (but it won't blow up if you connect it on not-very-wrong pins).

     

    The thing is: The BCM2836 processor is meant to be put into a digital camera, smartphone, or set-top-box. In each of these cases you MIGHT want a TV output, and the circuitry for that is easy-and-cheap on a chip. So that feature is included in the chip. But "TV signal input"  requires a much larger investment of chip-space and engineering efforts. Alas for you: it is not included.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to rew

    how do you know he doesn't mention it you are assuming image

    That's why I specified my assumption

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to Problemchild

    If you are thinking of the CCTV camera then most are composite and you can use one of those USB based Digitisers that are common on EBAY for around £10 ish

     

    Most have Linux support but I'm not sure if is compiled into t he RPI Kernel.

     

    Also it would be nice if you can tell us if it's a camera or monitor you are talking about

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Problemchild

    Hello John,

     

    Thanks for your sharing your thoughts and I apologize for the late response. I would like to verify that what I mean is the CCTV itself. The main camera. Could it be possible if I customize the camera itself so it can be compatible with the RPI 2?

     

    Divina

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rew

    Thanks Roger, I guess I really need to buy either converter or just replace the analog cctv with webcam which I think will be easier for me. Very much appreciated.

     

    Divina

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    Hi Divina,

     

    just an hypothesis: why don't use a CCYV camera that broadcast a 2.4 GHz short range radio signal (5-15 meters) then operate on the receiver nearby the PI ? Maybe a good compromise and IMO using a CCTV camera instead of a webcam you have more freedom to adopt specific cameras that are just though for this kind of use. Then from the composite signal you can isolate the video components for any usage (math, image processing etc.) There is a chip that I looked at and it is cheap (a cheap chip image ) and probably useful for your approach; it is used for very basic image processing from camera on Arduino so with the Raspi you just gain more and more power. It is a video synch separator in its three primary RBG components and it works fine:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to e14 Contributor

    Nope most probably  not have a look at those cheap USB VHS to DVD capture  cards as I said they are only around £10

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to Problemchild

    John Alexander wrote:

     

    how do you know he doesn't mention it you are assuming

    It's subtle. It was in the way it was worded that I picked up that the intent was to connect a camera.  But yes, maybe I was guessing, and guessed correctly.

     

    CCTV effectively has a 0.3 Mpixel resolution. I.e. when you wave your hand at the camera you can say: "Hey that's me, waving" when you watch the recording.  But when something actually happens, too often you end up with images that make it hard to recognize people.

     

    Nowadays cheap USB webcams can allow much higher resolution and thus better quality in case you end up needing the footage.

     

    With my raspberry pi camera extension kit, you could also get a 2 Mpixel video and 5 Mpixel-stills camera and then place it a few meters away from the 'pi. Less neat plastic packaging than with a webcam, but it will optimally use the hardware of the PI to say compress the fullHD stream to something you can archive.