Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum ras pi 4b no ALSA sound cards
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 702 subscribers
  • Views 8492 views
  • Users 0 members are here
Related

ras pi 4b no ALSA sound cards

rbdavis808
rbdavis808 over 4 years ago

Hi all,

I just installed the latest Void Linux release tarball (2021-09-30) onto my CanaKit Raspberry Pi 4 Model B w/4GB. Audio appears completely broken and I was not able to get it working by removing pulseaudio packages as recommended by another post in this forum. (I was unable to remove the libpulseaudio package due to excessive dependencies, but did remove pulseaudio, pulseaudio-utils and pavucontrol.) No sound is generated on either my HDMI monitor or the Pi's audio jack. I have traced this problem down to the fact that ALSA seems to think there are no sound cards in the system:

# aplay mysoundfile

ALSA lib confmisc.c:855:(parse_card) cannot find card '0' ...

(The alsamixer app generates the same error message.) Can anyone explain to me why ALSA can see no sound hardware on this system and how I can make it do so?

Thanks!

PS: There are no cards listed in /proc/asound and the /usr/bin/alsa-info.sh diagnostic generates the following relevant info:

Kernel release: 5.10.52_1

!!ALSA Version
!!------------

Driver version: k5.10.52_1
Library version:
Utilities version: 1.2.6

!!Loaded ALSA modules
!!-------------------

!!Sound Servers on this system
!!----------------------------

No sound servers found.


!!Soundcards recognised by ALSA
!!-----------------------------

--- no soundcards ---


!!PCI Soundcards installed in the system
!!--------------------------------------

!!Modprobe options (Sound related)
!!--------------------------------

snd_bcm2835: enable_compat_alsa=0
snd_bcm2835: enable_hdmi=1

  • Sign in to reply
  • Cancel
Parents
  • rbdavis808
    0 rbdavis808 over 4 years ago

    I was able to fix my problem after further web searches. My original installed /boot/config.txt contained the line

    #dtparam=audio=on

    Note that the line was commented out, thus apparently disabling audio. I had to uncomment it, and then the ALSA service installed from the VoidLinux alsa-utils package was able to detect both my HDMI and analog jack output devices.

    Curiously, /var/log/dmesg.log displays a kernel command line near the top of the file which includes the rather suspicious-looking option

    snd_bcm2835.enable_compat_alsa=0

    I did not make any attempt to change that, but perhaps dtparam=audio=on effectively overrides that?

    Hope others find this info useful, although perhaps it is specific only to VoidLinux.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rbdavis808
    0 rbdavis808 over 4 years ago in reply to rbdavis808

    PS: Just for grins I put back all of the pulseaudio packages I had removed earlier and then started the pulseaudio service.i.e., I now have both of the commands pulseaudio --system and alsa started at boot time. The only I app I really need to run is mpg123 -a outdev mp3file and that continues to work as before. I have no need for pulseaudio so I did not attempt to run any pulseaudio-specific commands.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rbdavis808
    0 rbdavis808 over 4 years ago in reply to rbdavis808

    PS: Just for grins I put back all of the pulseaudio packages I had removed earlier and then started the pulseaudio service.i.e., I now have both of the commands pulseaudio --system and alsa started at boot time. The only I app I really need to run is mpg123 -a outdev mp3file and that continues to work as before. I have no need for pulseaudio so I did not attempt to run any pulseaudio-specific commands.