Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Displaying a jpeg image with a RPI Pico
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 701 subscribers
  • Views 10218 views
  • Users 0 members are here
Related

Displaying a jpeg image with a RPI Pico

scottiebabe
scottiebabe over 3 years ago

It is easier than ever to display a jpeg image using Pimoroni's version of micropython https://github.com/pimoroni/pimoroni-pico 

The code is easy-peasy:

# Display an image on a pimoroni Pico Display
# -Scottie 2022
from picographics import PicoGraphics, DISPLAY_PICO_DISPLAY, PEN_RGB332
import jpegdec

# PEN_RGB332 is an 8 bit, fixed 256 colour palette which conserves your RAM.
# Try switching the pen_type to PEN_RGB565 (16 bit, 65K colour) and see the difference!
display = PicoGraphics(DISPLAY_PICO_DISPLAY, pen_type=PEN_RGB332, rotate=0)

# Create a new JPEG decoder for our PicoGraphics
j = jpegdec.JPEG(display)

# Open the JPEG file
j.open_file("e14scottie.jpg")

# Decode the JPEG
j.decode(0, 0, jpegdec.JPEG_SCALE_FULL)

# Display the result
display.update()

And, ta-da Tada

image

The image I used for reference:

image

The Image is 240x120 pixels and in jpeg format has a file size of 16 KB. 

Pimoroni have done a number of update to the Picographics python module in the last year. This image was displayed in a 332RGB color format. I am totally impressed how well the colors rendered with such a limited color depth. 

  • Sign in to reply
  • Cancel
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    scottiebabe Very Cool, I am impressed even though I have a distaste for Python and it's a throwback to Fortran. While it is very similar to C it has no end of a statement ala the; ie semicolon. This means more work on the programmer (me).

    I believe in structured code, but not this. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 3 years ago

    scottiebabe Very Cool, I am impressed even though I have a distaste for Python and it's a throwback to Fortran. While it is very similar to C it has no end of a statement ala the; ie semicolon. This means more work on the programmer (me).

    I believe in structured code, but not this. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to phoenixcomm

    I'm changing my mind on this. I'm still not a Python fanboy. But the more I look into well written Python project code, the more I get to appreciate it as a language.
    extra win: the libraries that are out there in the wild. 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to phoenixcomm

    I can live without the semicolons, but the use of indentation to mark off blocks really bugs me.

    Overall I still like it for fun quick projects, but I don’t think I would use it for anything serious. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to ntewinkel

    It bugs me too. But every language has things that rub me the wrong way.

    One day, you have to grow <>, and look at the values instead of the pet peeves.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to Jan Cumps

    I completely agree.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Jan Cumps

    Jan Cumps, My Gd. that's kind of nasty. Personally, I write in several languages. I will rate them and also tell you why.

    1. ANSI & K&R C. Great Language, Extensible, but easy to shoot yourself in the head if you are not careful. 
    2. FORTRAN is almost dead used a lot in aeronautics. 
    3. JAVA Nice language for building large software, interrupts are much easier than the C versions.
    4. PERL yes, this terrifies me but it has an sht-ld of a library. CPAN, variables are unitless! But for web dev and interfacing to DBM its worth the crud... one of my personal hatreds is the "my $varname; "
    5. APL neet language don't remember much of it. 
    6. Assembly Language(s) are all very similar, BUT DON'T GO NEAR  SPARC with over 100 registers to play with you better have a plan the C compiler is easier on the brain.  My favorite is the Motorola 6K stuff as it is still the only computer that was orthogonal. which means you can do this in one line of assembly code C++ = A++ * B--;  gee looks like C doesn't it. 
    7. Arduino IDE written in C++ is a mess! and Don't like it. And it scoping rules make me nauseous. 
    8. --- Python, get rid of the stupid intentions and add back in the dam ';" as the end of the line then I would use it. It reminds me of a C interpreter. 

    Jan instead of <> try >< and fly...